Bavaria's Best 50 - DEHN once again one of the best Bavarian SMEs

230725_pm_bayerns_best_50_dehn_pressebild.jpg

Christian Köstler (COO) and Florian Bohlmann (CFO) accepted the award on behalf of DEHN at Schloss Schleißheim.

More than 99 percent of German companies are small to medium size enterprises (SMEs). Not only do they account for around half of the country's total economic output. They also employ around 60 percent of the total workforce in Germany. Some of these companies stand out for their exceptional entrepreneurial drive and courageous plans for the future. Every year, the Bavarian State Ministry of Economic Affairs, Regional Development and Energy selects fifty exemplary Bavarian companies under the motto "Bavaria's Best 50" - and DEHN is once again one of this year's award winners.


Looking back over the past years, we can be really proud of what we have achieved together," says Dr Philipp Dehn, CEO of DEHN SE. “I am especially happy that all of our hard work has been honoured again this year: a truly magnificent team achievement! For me, this award both confirms many of the decisions we have made in the past and gives us new incentive for the tasks that lie ahead." Having won the award in 2019, this is the second time that DEHN has been honoured as one of "Bavaria's Best 50". 

Only owner-managed companies based in Bavaria are eligible for the award. In addition, the firms must have been in existence for more than five years and have less than 5,000 employees. Further criteria are that the companies can demonstrate a positive turnover and personnel development over the past five years.

Simon Thaler

Director of Corporate Communications