Protection concept against arc faults in the Charité Berlin

To maximise system availability and ensure the safety of the technicians, Charité opted for the DEHNshort arc fault protection system optimised for low-voltage switchgear installations.

Building of Charite, Hospital in Berlin

DEHN solution

Tested protection concept against arc faults

Customer

G. Klampfer Elektroanlagen GmbH

Project

Charité hospital building: 620 beds, 15 operating theatres, more than 100 clinics and institutes

Sector

Switchgear construction

Location

Berlin

Measure

Refurbishment

Investment volume

€202.5m

Construction period

2014 - 2016

Product

DEHNshort

The challenge

The Charité Mitte hospital building was extensively remodelled and completely renovated between January 2014 and November 2016. A complete overhaul of the electrical system also included the central low-voltage switchgear installation. Its failure, e.g. due to an arc fault, can cause considerable damage. All connected systems, including IT, can be affected and people can be seriously injured.

This is a danger that must be minimised, especially for the sensitive, networked and vital systems of a hospital. In order to maximise system availability and ensure the safety of technicians, protective measures are therefore essential components of the protection concept.

Störlichtbogenschutzsystem DEHNshort in der Charité Berlin

The solution

To meet these demanding challenges, Klampfer relies on the DEHNshort arc fault protection system, which is optimised for low-voltage switchgear installations. This consists of:

  • fibre-optic light sensors that detect the arc fault,
  • modular recording devices that process the signals,
  • quenching devices that quench the arc faults quickly and safely.

Arc faults are detected and eliminated as soon as they occur. The capability of the protection concept enables the affected switchgear to be recommissioned quickly. Long downtimes and the associated follow-up costs can be minimised.

Erwin Roither, Head of Distribution System Construction & Engineering, G. KLAMPFER Elektroanlagen GmbH

"Our customer, the Charité hospital in Berlin, opted for DEHNshort because the implemented protection concept ensures system availability and at the same time falls within the specified budget.
Thanks to the introduced arc fault protection system from DEHN, it was possible to dispense with the construction of additional battery rooms."

Erwin Roither
Head of Distribution Board Construction & Engineering, G. KLAMPFER Elektroanlagen GmbH, Leonding, Austria

Download reference

More references