Monitoring for wind turbine generator systems

Optimisation of maintenance and service thanks to lightning current measurement.

DEHNdetect is a lightning current measuring system that records both cloud-to-earth flashes and upward flashes. This condition monitoring system specifically for wind turbines transmits lightning data in real time and facilitates the optimisation of maintenance and service operations.  

Learn about the DEHNdetect lightning current measuring system and increase the availability of wind turbines.  

  • Real-time information
  • Optimised maintenance and service operations
  • Reduced downtimes
  • Optimised system cost efficiency
Monitoring of wind turbines
Lightning current measurement for wind turbines

Why is lightning current measurement needed for wind power systems?

Lightning damage to wind turbines – both onshore and offshore – often goes unrecognised, as it frequently does not cause immediate failure of the system. In the case of upward flashes, the initial long stroke current of only a few 100 A is the main cause of damage, such as melting on the receptors of the rotor blades. Damage like this must be recognised and rectified, as it can lead to system failure in the long term. 

Condition monitoring for wind power systems

To determine the intensity of lightning strikes, the IEC 61400-24 standard recommends the installation of measuring systems that also record long stroke currents. Keep a watchful eye on the parameters of a lightning event with DEHNdetect. This lightning current measuring system can be installed either at the base of the tower or at the transitions from nacelle to tower or hub to nacelle. It records both long stroke and impulse currents and automatically sends a notification after a lightning event. 
The blade detection feature indicates which rotor blade is affected, among other things. This means that maintenance work can be planned and optimally prepared on the basis of detailed data. 

Practical data management

The data are transmitted to a cloud via a mobile phone connection or via the wind turbine's local network. All the integrated lightning current measuring systems can be displayed individually here, and the parameters can be read out and managed. The option of connecting to various monitoring systems also safeguards flexible use in the future. Alternatively, data can be transmitted to a company's own servers.

The system records the following lightning current parameters: 

  • Impulse current [kA]
  • Long stroke current [A]
  • Charge [C]
  • Specific energy [MJ/Ω]
  • Rise time [kA/μs]

Lightning information services cannot measure upward flashes, known as ICC-only events, which are critical for wind turbines. This is where DEHNdetect comes into its own, as it also detects upward flashes – a clear advantage when documenting damage for insurance companies. 

Features of the DEHNdetect lightning current measuring system

  • Real-time information on lightning events
  • Optimisation of maintenance and service operations 
  • Prevention of subsequent damage
  • Reduction of downtimes 
  • Increased wind turbine service life
  • Optimisation of overall system cost efficiency

The measuring system components

Blade
detection unit

A total of up to nine units can be installed, including on other down conductors. 
They detect the lightning current of a lightning strike and transmit the lightning event to the data logger.

ICC IMP
measuring coil

This measures the impulse current as well as the long stroke current and transmits the measured data to the data logger. 

Data logger and measuring integrator

Measured data are analysed and important event data are determined here. The wind turbine operator receives an event-based notification.  The measured values can then be analysed subsequently. Visualisation of the measurement results takes place via the cloud-based DEHNsphere afterwards. 

Any questions?

We will be happy to clear these up in person.

Contact us

Relevant standards for lightning protection in wind turbine systems

IEC 61400-24 deals with the topic of lightning protection for wind turbines and contains detailed information on the selection of protection components. The installation of measuring systems that also record long stroke currents is recommended.

Downloads

FAQs

Services

We can provide support for your project from the planning to the implementation and beyond. Take advantage of our wide range of practical tools and services.

Any questions?

Write us a message.

I agree to the processing of my personal data in accordance with the Data Privacy Statement. Take me to the Data Privacy Statement.

 
Here you will find all information about the processing of your personal data.
CAPTCHA
This question tests whether you are human or a computer and prevents automated spam submissions.

What other topics are of interest to you?

Just select them and read on. 

Experience DEHNdetect Live at WindEnergy Hamburg

Discover how DEHNdetect supports condition monitoring and event management for wind turbines. Visit us at WindEnergy Hamburg, 22–25 September 2026, in Hall B6 | Booth 501.