DEHN Press

Portrait von Ute Pfister vor einem grauem Hintergrund.
Ute Pfister
Spokesperson for Trade Media, Surge Protection in Energy Technology, Lightning Protection/Grounding
+49 151 117 92 610
+49 9181 906-1295
ute.pfister@dehn.de
Portrait von Hannes Wolf vor einem grauem Hintergrund.
Hannes Wolf
Spokesperson for Trade Media, Surge Protection in Information Technology, Safety Equipment, Services
+49 160 31 74 927
+49 9181 906-3303
hannes.wolf@dehn.de
Simon Thaler
Simon Thaler
Director of Corporate Communications
+49 151 146 308 90
+49 9181 906 2339
simon.thaler@dehn.de

Latest posts

Year
Categories
✕

Image elecrama logo 1500x850px
DEHN showcases cutting-edge electrical safety solutions at ELECRAMA 2025

ELECRAMA is one of the largest electrical and power exhibitions for the Indian electrical industry and the largest standalone show in the electrical and allied equipment industry.High-performance lightning and surge protection is an integral part of safety concepts developed for many applications: industry, the supply of energy and raw materials, telecommunications and data centres. It minimises risks, ensures a constant flow of data and prevents damage or system failure. DEHN possesses huge expertise in the development and optimisation of lightning and surge protection concepts. This knowledge is also channelled into special engineering services like individual risk analyses and testing.At this year’s ELECRAMA from 22 to 26 February in the India Expo Centre & Mart in Greater Noida, Delhi NCR, DEHN can be found at Stand 8 in Hall 1 showcasing a wide range of products and protection solutions for futureproof plants and systems. Take a look at the latest innovative monitoring and control systems for predictive maintenance and real-time insights such as DEHNrecord SD EPMS and DEHNrecord SD CPMS.DEHN solutions increase the availability and service life of installations and systems. These include customised protection solutions for various industries, including oil & gas, telecommunications and renewable energies.DEHNrecord SD EPMS, for example, is a state-of-the-art system for monitoring and ensuring the effectiveness of earthing systems featuring real-time monitoring, remote access and intelligent diagnostics.DEHNrecord SD CPMS is a cathodic protection (CP) monitoring system for pipelines. It automates monitoring and allows pipeline operators to retrieve monitoring data as required. Real-time monitoring helps reduce corrosion-related risks and consequently extends the service life of pipelines while minimising downtime. Visit DEHN at ELECRAMA to learn more about these and other products. Discover customised solutions to meet your safety requirements. Meet the technical experts from DEHN face to face and discuss the challenges you encounter when it comes to lightning and surge protection, earthing, safety equipment and smart devices.Find out more on our website: https://www.dehn.in/en-in/elecrama 

Image 250122 DEHNcharge t1 batt 1500 fm 1500x850px
DEHNcharge: Customised surge protection for battery storage systems – essential for the future of energy supply

DEHN, the leading provider of lightning and surge protection solutions, presents DEHNcharge T1 BATT 1500 FM, a combined arrester for battery storage systems up to 1,500 V DC. Large-scale battery storage systems play a key role in the modern energy landscape. They enable the efficient storage and supply of energy from renewable sources such as wind and solar energy. To ensure the reliability and longevity of these storage technologies, effective protection against overvoltages is essential. Lightning strikes or switching operations in the grid cause surges that can damage sensitive electronic components in storage systems. Appropriate protective measures are therefore crucial to avoid failures and high repair costs. Sophisticated surge protection safeguards your investment in storage technology and contributes to the stability of the power grid.DEHNcharge T1 BATT 1500 FM is a DC surge protective device for battery storage systems up to 1,500 V DC. The product complies with EN 61643-11 and is classified as a Type 1+2 arrester. The maximum continuous voltage is 1,500 V DC. The lightning impulse current per pole is 5 kA. The protective device can withstand a short-circuit current of up to 100 kArms (ISCCR) if a maximum backup fuse is used.The prewired Type 1 + Type 2 combined arrester for large DC battery storage systems is characterised by the tried-and-tested, fault-resistant Y circuit. At just four standard DIN modules, the design of the enclosure is compact. It can be seamlessly integrated into systems up to 1,500 V DC.The DEHNcharge has a maximum protection level of ≤3 kV. It can be used with a prospective short-circuit current of up to 100 kA. This surge arrester is therefore able to work reliably even with very high short-circuit currents, which significantly increases the safety and longevity of the battery storage system.A function and fault indicator is provided by a green-red marking in the inspection window, which makes the current status of the device visible at a glance.You can find the technical details here.

25.10.2024

Image Sustainability Report EN 1200 x 1200 px
On course for a sustainable future – DEHN publishes its first Sustainability Report

DEHN is embarking on a transformation, focusing strongly on ESG principles and aiming to set new standards for protecting humanity, the environment and companies. The family-owned company explains with its Sustainability Report how it is embracing the energy revolution and decarbonisation while encouraging customers and partners to do the same, with efficient energy management and use of renewable energy sources at the heart of the company’s strategy. As Dr Philipp Dehn, CEO of DEHN SE, says: “Sustainability is a marathon, not a sprint. We’ve been proving we have the stamina since 1910”.From 2025/26, DEHN will be required to comply with the EU’s sustainability reporting obligations. The company is getting ahead of the game now by voluntarily publishing its first Sustainability Report to create transparency for customers and employees. The report shows the current status and the planned measures for greater sustainability. In the 2023/2024 reporting period, DEHN developed a comprehensive sustainability strategy and decided on a sustainable and cooperative approach to tackle the four central areas of action identified. DEHN believes in forward-thinking partnerships based on trust and shared values, whether in managing the business, acknowledging its obligations as an employer, taking responsibility for products and services or showing commitment to environmental issues. In future years, DEHN will take an even more professional approach to sustainability management, in particular with ESG indicators and objectives. Commitment to and interest in sustainability should be encouraged among the workforce. The foreign subsidiaries will also be actively involved to achieve global consistency and a common understanding of sustainability goals. In-house communication will be intensified to inform and include staff better. The dialogue with partners along the value chain, will also be deepened and expanded, especially on subjects such as the circular economy. Climate protection, in conjunction with advanced energy management, will always be a top priority for DEHN. The company utilises energy from renewable sources with PV systems at the sites in Neumarkt and Mühlhausen as well as a combined heat and power station. DEHN obtains the rest of the energy required in the form of climate-neutral green electricity and green gas. The rapid pace of technological, economic and environmental change demands continuous learning and development of new skills. True to the motto “lifelong learning”, DEHN is committed to long-term personnel development. Future updates will explain both the progress made and the stumbling blocks encountered – our first 2023/24 Sustainability Report can be viewed here.

24.10.2024

241024_pr_dehnguard_ez-s.png
Introducing the DEHNguard EZ50-S: Superior Surge Protection with Unmatched Serviceability for AC Power Installations

Mooresville, NC – October 24, 2024: DEHN, a global leader in lightning and surge protection, announces the launch of the DEHNguard EZ50-S. This cutting-edge Type 1 NEMA 4X surge protective device (SPD) sets a new benchmark in the industry, offering exceptional surge protection and unparalleled ease of maintenance. It is the ideal AC power protection solution for multiple applications, ranging from industrial and commercial buildings, data centers, process technology, energy supply and water/wastewater plants, to mobile phone sites and green energy systems such as the electric vehicle charging infrastructure or battery storage systems. The DEHNguard EZ50-S is a cost-effective solution designed to enhance system reliability and avoid unnecessary downtime.The DEHNguard EZ50-S is engineered for both outdoor and indoor installations. The robust enclosure, specifically designed to endure hard outdoor conditions, offers reliable protection against environmental factors and meets NEMA 4X and UL50E Type 4X standards.  Featuring globally recognized MOV technology with thermal sensing disconnection, the SPD offers a maximum discharge current rating of 50 kA (8/20 µs) per phase. It is UL 1449 5th Edition approved with a short circuit current rating SCCR of 200 kA and requires no additional overcurrent protection.  Designed for easy maintenance and installation, the compact DEHNguard EZ50-S comes with 10 AWG, 36" long cables for straightforward connections and flexible mounting options. The SPD is prewired for streamlined installation and features visual status indicators for simple monitoring and maintenance. The field-replaceable plug-in modules allow for quick and easy maintenance without the need to disconnect power, reducing downtime and minimizing the total cost of ownership. "The DEHNguard EZ50-S stands out for its top-notch protection and exceptional ease of maintenance," says Mike Bayda, Product Manager for Surge Protection Devices at DEHN, Inc. "Its maintainability is crucial for critical infrastructure, ensuring long-term reliability and cost savings." The DEHNguard EZ50-S is proudly made in the USA and now available to order. For more information or to place an order, please visit www.dehn.us or contact DEHNsales@dehn.us.

17.10.2024

image whats new 1600x900 px
Northern European Expansion: DEHN founds subsidiary in Norway

DEHN, the specialist for lightning and surge protection and safety equipment, has been doing business in Northern Europe for over thirty years. Having established its own companies in Denmark and Sweden, the group is now expanding its business opportunities in Northern Europe by founding a new subsidiary in Norway.Norway is one of the most prosperous countries in the world with the second highest standard of living after Iceland. The Norwegian economy is strongly influenced by the oil and gas industry, as well as extensive investments in renewable energies. This combination perfectly matches the strategic segment orientation at DEHN and opens a wide range of opportunities for the company.Consequently, DEHN NORGE was established in Oslo in September. With this step, the company also aims to provide customers in Norway with a comprehensive portfolio which includes local consulting expertise and specialist training. Fredrik Hem-Andersen, who has over 20 years of experience in product management and sales in the Norwegian electrical industry, took up his position as Managing Director of the new subsidiary on 1 October 2024. “With his in-depth knowledge of the market and industry, Fredrik Hem-Andersen will play a crucial role in driving forward our expansion in Northern Europe,” says Boris Wolff, CSO DEHN SE.Mr Hem-Andersen is also the chairman of the standardisation committee for lightning and surge protection at the Norwegian Electrotechnical Committee (NEK).

20240903_pm_dehn_auf_der_innotrans.jpeg
InnoTrans 2024: DEHN protects the railway infrastructure

Modern interlockings use digital network technology to transmit control commands to points, signals or track contacts. On the one hand, this increases the efficiency and reliability of the system. On the other hand, the high proportion of electronic components is susceptible to disruptive influences such as overvoltage and lightning strikes. DEHN's interlocking protection solutions, which comply with the guidelines and are approved by DB InfraGO AG, protect interlockings against failures and thus safeguard railway operations. Modern technologies, innovative products and convincing solutions bring more safety to railway infrastructure and thus also to mobility. At this year's InnoTrans, which takes place from 24 to 27 September in Berlin, DEHN will be offering an insight into its wide range of products and solutions for the railway industry at Stand 320 in Hall 21. DEHN provides the rail sector with a coordinated range of products, solutions and services such as external and internal lightning protection, surge protection, equipotential bonding, earthing measures for buildings and railway systems, safety equipment and other services, including lightning protection planning and laboratory tests.  For maximum system availability: DEHNventil ACIHigh demands are placed on the availability of switchgear – for example in railway interlockings. This makes surge protection essential. And changing surge protection modules should not compromise system availability. The new DEHNventil ACI M TNS 264 FM has no backup fuse and is flexible in terms of its application. The touch-safe design allows the protection module to be replaced without system downtime. The ACI technology employed also enables connection cross-sections of just 16 mm2. This facilitates installation and saves time.DEHNcare ArcFit – The personal protective equipment (PPE)DEHNcare ArcFit is light, comfortable and safe protective clothing. It meets arc flash protection class APC°2 and fulfils high-visibility clothing class 3. The protective clothing is also designed to be comfortable and suitable for everyday use. DEHNsense EFD – More safety when working on electrical installationsThe DEHNsense EFD, a voltage detector that can be worn on the wrist or helmet, completes the protective clothing. It provides visual, acoustic and haptic warnings of the dangers of electric current by detecting a critical AC voltage and alerting the user in good time before entering the immediate danger zone. As an additional measure to the 5 safety rules, the detector can significantly increase safety when working on electrical systems. All relevant events are logged in the DEHNwork app, which enables complete documentation.Check the condition of overhead lines easilyThe DEHNproX wireless inspection camera enables safe and efficient inspection of switchgear and overhead contact lines in the railway environment. The inspection can be carried out without disconnecting the systems, which increases operational safety and minimises downtimes. The practical inspection camera with DB InfraGO AG approval thus facilitates the regular visual inspection and documentation of the condition of the live overhead contact line system. This contributes significantly to the safety and reliability of the railway infrastructure by enabling potential hazards to be recognised and rectified at an early stage.

Image ICLP 2024 Dresden EN 1500x850px
DEHN SE shares its expertise in lightning protection at the ICLP 2024 in Dresden

Neumarkt, August 2024 - DEHN is looking forward to participating in the 37th International Conference on Lightning Protection (ICLP) 2024. The prestigious conference in Dresden from 1 to 7 September brings together experts and specialists from all over the world to discuss the latest developments and research results in the field of lightning protection. With a total of nine technical contributions, DEHN helps to create a specialist platform where international scientific and technological experts can exchange ideas and address the challenges of the future together.As a pioneer in lightning and surge protection technology, DEHN can contribute over 100 years of experience and innovation to the industry. With a broad portfolio of products and services, the company sets benchmarks in quality and reliability. One example of this is ACI technology: the innovative Advanced Circuit Interruption (ACI) technology ensures reliable and durable surge protection, and its integrated switch/spark gap combination eliminates the need for an external back-up fuse."We are proud to be a Gold Sponsor at ICLP 2024 and to share our expertise in the field of lightning and surge protection," says Christian Höhler, CTO of DEHN SE. "This conference offers an excellent platform to exchange ideas with international experts from science and technology and to work together on solutions to meet both current and future challenges."  

12.08.2024

image whats new 1600x900 px
USA: DEHN, Inc. enters strategic partnership with BBP

DEHN, Inc. enters strategic partnership with BBP to further expand lightning and surge protection solutions in the South/Southeast US Mooresville, NC - DEHN, Inc., a global leader in lightning and surge protection solutions, is entering a strategic partnership with BBP, a distinguished provider of instrumentation, valves, analytical products, and control systems, to enhance protection offerings across the South/Southeast region of the United States. Through this collaboration, customers in the region can now benefit from the combined strengths of DEHN and BBP, accessing a comprehensive range of protection solutions designed to meet the unique needs of various industries. DEHN's world-class lightning and surge protection solutions are designed to protect against surge events and transient voltage, safeguarding vital infrastructure and enhancing the resilience of electrical networks. By combining DEHN's expertise in surge protection with BBP's deep regional knowledge and customer-centric approach, this partnership will pave the path forward for enhanced infrastructure protection and longevity. "Partnering with BBP is an exciting step for DEHN as we continue to expand our footprint in the US market," said Ryan Fitzgerald, VP of Sales and Marketing at DEHN, Inc. "BBP's reputation for excellence and their extensive network will be invaluable as we work together to provide high-quality, reliable protection solutions to businesses across the South and Southeast." Scott Romero, President at BBP, echoed this enthusiasm, stating, "I'm confident that the partnership between BBP and DEHN will greatly enhance the value we deliver to our customers, providing them with more comprehensive and tailored solutions. This collaboration allows us to better meet their needs by leveraging the strengths and expertise of both companies." The partnership reflects DEHN’s and BBP’s shared dedication to advancing safety and innovation by bringing cutting-edge protection technology to an even broader audience. 

25.07.2024

image whats new 1600x900 px
DEHN to acquire parts of ABB’s surge protection business in the USA

Rapid electrification, the expansion of renewables and the increasing popularity of megatrends such as e-mobility open up new business opportunities around the globe, particularly for the electrical industry. In the light of this, the United States remains a high focus market, not least because of extensive government investment programs. In order to maintain a leading position in the region, DEHN is acquiring parts of ABB's surge protection business in the US. “International growth is central to the continued positive development of our company,” says Dr Philipp Dehn, CEO of DEHN SE. "The US market offers us a range of attractive business opportunities that we can now address even faster and on a wider scale thanks to the expertise and excellent market position of the Current Technology and Joslyn brands." DEHN is stepping up its activities in the United States. In the spring of 2024, DEHN Inc. moved its headquarters to Mooresville, North Carolina. This will be the base for driving business development throughout the country and region as well as for establishing a production facility for the American market. In this context, the current acquisition acts as an additional catalyst for DEHN’s goals in the US and the rest of the Americas. “In combination with our existing portfolio, the addition of Current Technology and Joslyn low-voltage products creates a unique offering for our customers in the US in the areas of power quality, grounding, lightning protection and surge protection," explains Ingo Rutenberg, CEO DEHN Americas. "From planning to the installation and maintenance of lightning and surge protection solutions, we can now cover a wide range of applications and tackle the problems faced by our customers in a targeted and customized manner."Both Current Technology and Joslyn are well-established and respected brands in the American market, which operate to date as part of ABB. In addition to the corresponding product portfolio including IP, the acquisition also includes a dense network of long-established sales partners in the United States. Both parties have agreed not to disclose the financial details of the acquisition. Completion of the transaction is scheduled for Q1 2025. From this time onwards, all surge protection products under the names of Current Technology and Joslyn will be manufactured and distributed by the existing subsidiary DEHN, Inc.

26.06.2024

image whats new 1600x900 px
Bigger footprint in Asia: DEHN founds subsidiary in Japan

DEHN steadily continues its course of international growth and emphasises the strategic importance of the island nation of Japan by establishing a new subsidiary there. DEHN’s smart protection solutions, especially for the expansion of regenerative energies or telecommunications, have been well received in the Japanese market. "Global megatrends such as renewable energies, electric mobility and digitalisation are key drivers of our growth in recent years. After all, energy networks of the future can only function reliably with appropriate protection solutions. And it is precisely these solutions that we have to offer," says Dr Philipp Dehn, CEO of DEHN SE: “By choosing Japan as a location, we are reaffirming our commitment to quality and safety in a country that itself sets high standards in lightning and surge protection and drives forward innovative energy solutions.” With "Japan's Roadmap to Beyond-Zero Carbon", the ambitious nation is following the megatrend of decarbonisation and aims to drastically reduce carbon emissions by 2050. The focus here is on the expansion of sustainable energy, such as photovoltaics, wind energy and hydrogen technology, as well as the telecommunications sector. The new DEHN subsidiary will therefore concentrate on these key industries, making a significant contribution to protecting critical infrastructure. Local presence will also enable DEHN to offer customised solutions to meet the specific requirements of the Japanese market. The subsidiary based in Yokohama, will operate under the name DEHN JAPAN K.K..