Prefabricated houses from KAMPA

KAMPA stands out for its strong sense of responsibility for the environment. Houses are made of wood, an ecologically sustainable building material. 

And genuine energy-plus houses are the actual production standard. In line with its commitment to quality, KAMPA relies on solutions from the experts at DEHN for surge protection.

Single family house

DEHN solution

Protection concept for single-family and multi-family houses in prefabricated construction

Customer

KAMPA GmbH

Sector

Prefabricated house

Products

DEHNshield ZP Basic, DEHNbox, DEHNgate, DEHNcube, DEHNgate 5FFTV, DEHNflex, DEHNprotector

The challenge

KAMPA energy-plus houses are equipped with the innovative energy and climate solution from Viessmann as standard. In addition to a climate-friendly heat pump with heat recovery, floor heating and cooling in summer and the VIESSMANN ventilation system, which also regulates the humidity, it also includes a photovoltaic system with battery storage and energy management.

It is particularly important that this networked system is optimally protected in the event of a thunderstorm. This is because the overvoltages resulting from a lightning strike can pose a danger to electrical and electronic components.

Einfamilienhaus von KAMPA

The solution

KAMPA has therefore opted for a reliable protection concept from DEHN. The overvoltage protection is integrated into the bus system of KAMPA prefabricated houses. As standard.

The house connection (incoming power supply lines) is protected with the DEHNshield ZP Basic combined arrester. DEHNgate FF5 TV protects the cable and broadband connection and DEHNbox, alternatively DEHNgate, was selected for the telephone/DSL connection. DEHNcube also protects the inverter in the photovoltaic system.

In this way, KAMPA ensures a consistent energy and data supply, as well as efficient energy management of the houses. Even after a thunderstorm.

KAMPA GmbH
Single-family house from KAMPA
DEHNshield ZP Basic
Building Innovation Center KAMPA
DEHNbox
Single-family house from KAMPA
Single-family house from KAMPA
Single-family house from KAMPA
Single-family house from KAMPA
Single-family house from KAMPA

More references