DEHNdetect in practice

DEHNdetect in use on the Gaisberg

The DEHNdetect lightning current measuring system supplies valuable data for research activities on the Gaisberg.
It reliably and comprehensively records all lightning currents – even those with low current impulses, as they occur in ICCOnly events, for example. This is an important consideration, because a large proportion of the lightning events on tall objects – as is the case on the Gaisberg transmitter – are so-called upward flashes. They often have impulses under 1 kA, and conventional lightning detection systems mostly cannot map them.

Multiple lightning bolts striking near a city skyline at night, with dark storm clouds illuminated by flashes of light.

Team Gaisberg

Dr. Dipl.-Ing. Wolfgang Schulz – Director of OVE Service GmbH, ALDIS (Austrian Lightning Detection & Information System)
Dr. Dipl.-Ing. Gerhard Diendorfer – OVE Service GmbH, ALDIS (Austrian Lightning Detection & Information System)
Dipl.-Ing. Hannes Pichler – OVE Service GmbH, ALDIS (Austrian Lightning Detection & Information System)
Dipl.-Ing. Hannes Kohlmann – OVE Service GmbH, ALDIS (Austrian Lightning Detection & Information System)
Johann Breyner, BSc. – OVE Service GmbH, ALDIS (Austrian Lightning Detection & Information System)
Tall red-and-white transmission tower with multiple antenna dishes beside a building, set against a clear blue sky.

About the Gaisberg

The Gaisberg is one of the most striking landmark mountains of Salzburg and is 1,287 m high. A transmission station is located on top of it, which is one of the places in Austria most often struck by lightning. It therefore represents the perfect location for measuring and researching lightning currents.

Lightning research on the Gaisberg

The transmission and radio tower on the Gaisberg is used by ALDIS (Austrian Lightning Detection & Information System) for lightning research. Different lightning current parameters are determined using modern measurement technology as part of the research activities. The following measurements have been performed over the past few years:

  • Direct measurement of lightning current amplitude with a shunt from 1998–2018
  • Indirect measurement of lightning current amplitude with a Rogowski coil from 2020 to present
  • Determining the charge of the individual impulses and the total charge of a lightning strike
  • Transient electrical field measurement with plate antennae during a lightning stroke at a distance of 170 m and 130 km
  • Measurement of the electrostatic field with a field mill
  • Measurement of meteorological data (temperature, air pressure, wind speed)
  • Rain measurement with micro rain radar and disdrometer

The transmission mast and the data collected here also provide the perfect opportunity to check the quality of the ALDIS lightning detection system: time, location and lightning amplitude are precisely noted through the measurements. These details can then be compared with the available ALDIS data and potential discrepancies can be identified.

DEHNdetect delivers new findings

DEHNdetect has been in use on top of the Gaisberg since 2021. The lightning current measuring system detects all types of lightning currents: impulse currents and dangerous long stroke currents. Thanks to the high precision of DEHNdetect, the system supplies reliable data, thus contributing substantially to the research project.

Measurement examples

Line graph with a blue curve showing a steep drop, fluctuating low values, and a gradual rise over time, with gridlines and numeric axes.

ICC

ICC (initial continuing current) without pulse currents.

Line graph with a red curve showing a sharp downward spike and gradual recovery over time, gridlines and numeric axes visible.

Downward flash

Example of a rare recording of a downward flash into the Gaisberg transmission tower

More questions?

Marjan Valand
Business Development Manager at DEHN
Portrait of a man with short dark hair and gray goatee, wearing a suit and red striped tie, smiling at the camera
+49 9181 906 1505
marjan.valand@dehn.de