Surge protection for LED lighting
The use of efficient LED technology is now widespread when building new street lights or retrofitting existing ones. Compared to high-pressure sodium vapour lamps or fluorescent lamps that have been used up until now, LED illuminants are an alternative that saves both electricity and CO2. In addition to energy efficiency, the significantly lower maintenance intensity is also a real plus point.
However, if you are responsible for planning or supplying street lighting, you will also face challenges. Compared to conventional lighting technology, LEDs have a lower interference immunity to surges. Powerful surge protection is therefore essential, both to protect your investment and to avoid the costly replacement of illuminants. Find out here how we contribute to the reliable operation of LED street lights with sophisticated surge protection concepts.
How we protect LED mast lights against surge damage
Surges caused by direct or indirect lightning strikes usually lead to partial or complete failure of the LED modules, destruction of the LED drivers, reduced brightness or failure of the entire control electronics. And even if the LED light initially remains functional after an overvoltage event, its service life can be significantly reduced as a result.
With an effective surge protection concept, you can avoid unnecessary maintenance work and ensure availability.
In the distribution box: the prewired DEHNshield is the first component of a holistic protection concept. The Type 1 + 2 spark-gap-based combined arrester is available with a floating remote signalling contact – this allows faults to be detected at an early stage and appropriate measures to be taken.
In the lamp pole: we have developed various options to protect the light point from overvoltage. The EK480 fuse box is the system solution for a new light point for installation inside the mast.
Ideal alternative for retrofitting: the compact Type 2 + 3 surge arrester DEHNcord L 3P, which has been optimised especially for confined installation situations in the fuse box.