DEHN Pressemitteilungen
Press releases

September 2021

DEHNrecord Smart Device - Creating transparency in a low-voltage system

Modern power grids consist of an increasing proportion of electronics and therefore have many components with a low dielectric strength. They are also highly interconnected. Added to this is the shift from centralised power generation to a volatile power grid supplemented by a multitude of decentralised renewable energy generators and non-linear power consumers. 

July 2021

DEHNventil: Full Power - half the width

In just 4 standard DIN modules, the compact combined arrester, type 1+2+3, protects against transient overvoltages in low-voltage switchgear and controlgear assemblies. Small width and a compact single module that saves you time during installation and maintenance. The arrester boasts another strength with its RAC spark gap. It reacts extraordinarily quickly and with the lowest residual energies minimises the impact on downstream electronic installations and systems. 

DEHNventil – how to keep systems available and processes running. 

January 2021

DEHNcare ArcFit – Individual configuration, greater comfort, reliable protection.

With the new arc-fault-tested DEHNcare ArcFit protective clothing and the corresponding online configurator, DEHN offers more individuality and comfort during the highly demanding task of working on electrical installations. With the new, user-friendly configurator, you are only a few clicks away from the desired protective clothing. In addition to the choice of size and colour, it can be customised with your own logo and name. DEHNcare ArcFit is a new collection of multinorm protective clothing developed to protect the wearer in various working conditions, for example, against arc faults, heat and flames and electrostatic charge. This comfortable, sporty and customisable protective clothing is part of the range of personal protective equipment against the thermal effects of an electric fault arc. Wearers also act as ambassadors for their own brand.

DEHNcare ArcFit is sporty, comfortable, customisable and above all safe.

December 2020

DEHNdetect - Quick as a flash, strikingly smart and at the same time flexible and easy to install

Wind power makes a sizeable contribution to the total power generated from renewable energy sources. The installation and operation costs must be amortised over the average 20-year operating phase of these plants. In order to do this, the entire lifecycle of the plants must be continually optimised and adjusted to changing circumstances, technological or economic. Constant monitoring and foresighted maintenance are essential. This is where DEHNdetect comes into play. This new lightning current measuring system reliably detects lightning events both on- and offshore. It has a large measuring range and can therefore also detect the long stroke component of the lightning current which is often responsible for melting rotor blades due to its high charge. DEHNdetect is flexible since it is modular in design and easily retrofitted.

November 2020

Christian Höhler becomes CTO at DEHN

Christian Höhler becomes CTO at DEHN

The family-owned company DEHN has appointed Christian Höhler as CTO as of 01 November 2020. The 51-year-old graduate engineer can draw on many years of experience in the international environment as a development and sales manager. At WERMA, one of the market leaders in the field of signalling in industry and buildings, he was latterly responsible for the Research and Development section.

March 2020

BLITZDUCTORconnect - Easy. Safe. Robust.

The combined lightning current and surge arresters of the new BLITZDUCTORconnect series protect automation and measuring and control systems in industrial environments as well as information technology interfaces. A high lightning current discharge capacity and a low protection level make them ideal components for reliable terminal device protection. They are available in a compact or modular design and both variants have a width of only 6 mm. Functions such as the new secR release buttons and push-in technology help to minimise the installation effort.

The status indicator and a compatible remote signalling unit immediately report any failure in case of overload. Ex-approved versions of BLITZDUCTORconnect are available for intrinsically safe signal circuits.

September 2019

Family business DEHN on international course

With this clear company designation DEHN, as a leading supplier of lightning and surge protection and safety products and solutions, clearly underscores its importance as a globally active company and promotes the sustainable development of the DEHN brand.

August 2019

Whether small rooftop PV systems or multi-megawatt systems - DEHNcombo protects!

The new DEHNcombo YPV combined arrester from the lightning and surge protection specialist DEHN safely protects PV systems from surges caused by lightning interference. The arrester offers a number of application advantages for PV systems in a single device. The varistor-based protective device combines a type 1 lightning current arrester and a type 2 surge arrester and incorporates a tried and tested Y circuit.
DEHNcombo YPV efficiently protects the DC side of the inverter, the combiner box or the PV modules. This new arrester can be used for small rooftop systems, but also for systems of the multi-megawatt class.

April 2019

Smart and safe with DEHN

The sustainable use of resources requires the intelligent and sustainable generation, distribution and use of energy. This includes protection of the associated systems and plants. At “The Smarter E Europe“ (hall B3, booth 372) - the most important industry platform which takes place from May 15 to May 17 in Munich - we will demonstrate how to protect systems against lightning-related surges and safely handle electrical energy. The event brings together four exhibitions under one roof: Intersolar, Power2Drive, ees and EM-Power, making it the largest energy trade fair in Europe. Under the motto “DEHN protects.“, DEHN will present innovative protection solutions for photovoltaic systems, smart grids, battery storage systems and e-mobility, irrespective of the plant size. Based on practical protection solutions, the DEHN experts will explain how lightning and surge protection can increase the availability of photovoltaic systems, including the grid infrastructure and battery storage systems, or the e-mobility charging infrastructure.

March 2019

Wireless inspection camera brings the invisible to light

The wireless inspection camera by DEHN is now available with an optional LED lighting unit which is quite simply mounted to the camera enclosure. The practical camera is ideal for inspecting and documenting the state of electrical installations up to 123 kV / 15-60 Hz – under live conditions. The extra lighting, point or diffused, makes it possible to use the camera in badly lit locations. It is simple to control via WiFi and an app on a smartphone or tablet computer. Safe operation is a simple matter, without any special training on the part of the electrician. The photos and documentation transmitted live can be saved and forwarded.

December 2018

HVI – modern lightning protection for today and tomorrow

Neumarkt – Mid-December 2018: DEHN greeted over 30 lightning protection installers from all over Germany. “DEHN is already in its fourth generation and still fascinated by the phenomenon lightning, our passion. Like previous generations, we look for opportunities to meet future challenges and make the world a little bit safer through our own protection solutions and the skill of the lightning protection installers. It is our common experience in trade and industry which flows into the further development of lightning protection” said Dr Philipp Dehn in his speech on the topic: 15 years of HVI. DEHN brought its guests up to date on the development and testing of the HVI high voltage resistant insulated conductor and technical innovations and trends in the field of lightning protection. A visit to the high voltage laboratory at the Technische Hochschule Nürnberg Georg Simon Ohm rounded off the technical framework programme.

November 2018

Spark gaps in ex areas – easy installation and testing thanks to coaxial connection technology

The EXFS Coaxial Connection Box by DEHN is the ideal solution for integrating
electrically conductive parts in ex areas like, for instance, the insulating joints of
pipelines, in the lightning equipotential bonding.
This effectively protects those electrically conductive parts in ex areas which
cannot be directly interconnected against lightning induced surges.
The benefits for the user, above all, during installation, maintenance and testing
are significant. The Coaxial Connection Box is installed above the ground so that
the regular inspection of the integrated EXFS 100 can be conducted outside the
ex area. There is also no need to disconnect cables or remove insulation when
testing. What is more, mounting is simple because DEHN includes all fixtures and
assembly accessories in the scope of delivery.

October 2018

ACI technology by DEHN – Device safety redefined

Safe dimensioning makes the new DEHNguard with ACI technology (Advanced Circuit Interruption)a no-worries package for the user who saves space, time and costs. ACI technology presents a technical solution to dimensioning issues which eliminates the need to select the right back-up fuse or conductor cross-section. ACI fulfils the requirements of tomorrow today. Constant availability of electrical systems is a must. Power cuts and system failure are out of the question. Now and in the future, it is important to consider the ongoing transition in the global power supply. Renewable power generation is creating new grid parameters: Isolated grids and storage systems are changing the short-circuiting conditions. One aspect which the new ACI technology already has well under control.

August 2018

DEHN protects the railway infrastructure

Be it with lightning and surge protection for electronic and digital interlockings, for level crossings or point heaters - “DEHN protects the railway infrastructure”. With this motto, DEHN will be at InnoTrans, the leading international fair for transport technology, in Berlin from 18th to 21st September, 2018. At stand 218 in hall 11.1, DEHN will feature practical lightning and surge protection solutions with which to prevent costly downtime and operational disruptions. The experts at DEHN will provide information on individual solutions, the seminars available at the DEHNacademy and the testing services offered in the laboratories.

May 2018

DEHN at the Intersolar Europe 2018

All safe – one flash ahead of the storm

From 20 – 22 June you will find DEHN at the leading platform for the solar industry -  the Intersolar in Munich, hall A2, stand 536. Whether kilowatt or megawatt systems, DEHN protects your investments across the globe against interruptions caused by lightning currents and surges. Practical solutions show how lightning and surge protection can increase the availability of photovoltaic systems in conjunction with the network infrastructure, battery storage or electromobility.

May 2018

Compact 5-channel arrester for SAT systems

The new surge protective device DEHNgate FF5 TV is suitable for universal application in analogue and digital SAT systems. One arrester can protect analogue or digital satellite reception systems with, e.g., a quad LNB (multi-switch) plus a terrestrial antenna.

May 2018

Protective shield against high-pressure water jets – DEHNcare WJP

Personal protection takes top priority when using high pressure water jets for cleaning purposes. The right protective clothing minimises the risk of accident and injury. Beside occupational safety considerations, personal protective equipment (PPE) should be comfortable to wear and provide sufficient freedom of movement. The new DEHNcare WJP overall fulfils both requirements – safety at work and comfort. The high-pressure water jet protective overall has been tested in accordance with recognised test principles (test pressure 1,200 bar) to reliably withstand water jets of up to 1,000 bar. Moreover, the innovative lightweight material does not restrict movement and is therefore comfortable to wear.

April 2018

Surge protection that defies wind and weather

DEHNpatch outdoor is the new complete unit comprising surge protection and an enclosure for outdoor use. With IP 66 degree of protection, a universal mounting bracket (horizontal/vertical, pole or wall) and transmission class E, the new surge arrester DEHNpatch outdoor is the perfect protective device for Ethernet applications (also PoE++) in outdoor areas.

February 2018

DEHN opens a national subsidiary in the Netherlands

DEHN continues to focus on the internationalisation of sales activities. DEHN has been active in the Netherlands for decades. In January, it opened its own company DEHN NEDERLAND B.V. in Amersfoort. The aim is to intensify marketing activities and support customers when marketing on a local level.

February 2018

Thrilling Times

Due to digitalisation, networked technology is becoming more important, equipment and components more sensitive and demands in the workplace higher. Failure of sensitive, networked technology is unthinkable and often has dire consequences.
“Connected – Secure – Convenient”, the motto of this year’s Light + Building, has also been taken up by DEHN whose stand D90 in hall 8.0 at the international trade fair for light and building technology in Frankfurt/Main from 18 – 23.03.2018 will show how to cope safely and simply with any challenges to be met in the thrilling times in which we live.

January 2018

DEHN now accredited by DAkks

At the end of 2017, the DEHN Test Centre was awarded an accreditation certificate (Registration number D-PL-20356-01-00) by the Deutsche Akkreditierungsstelle, DAkkS (German accreditation body). For DEHN this is further objective proof of the quality and competency of its testing.

January 2018

DEHN is committed to protecting the environment and resources

DEHN not only develops protective devices for the regenerative power generation sector, but actively promotes the use of sustainable power at its locations in Neumarkt and Mühlhausen. Solar energy and a combined heat and power plant are already used to generate electricity and provide warm water. In January, a new photovoltaic system was put into operation at the premises in Mühlhausen, producing approx. 750,000 kWh of additional electricity annually. This leads to a CO2 saving of some 350,000 kg per year. In this way, DEHN makes an important contribution towards protecting the environment and resources.

Petra Raab

Your contact

Petra Raab ⎟ Corporate Communications

Phone: +49 9181 906 1426

Eva-Maria Kerschensteiner

Your contact

Eva-Maria Kerschensteiner ⎟ Corporate Communications

Phone: +49 9181 906 2097

Are you looking for a previous press release?

back to top

Cookie Settings

We use cookies so that we can offer you the best possible website experience. This includes cookies which are necessary for the operation of the website and to manage our corporate commercial objectives, as well as other cookies which are used solely for anonymous statistical purposes, for more comfortable website settings, or for the display of personalised content. You are free to decide which categories you would like to permit. Please note that depending on the settings you choose, the full functionality of the website may no longer be available. Further information can be found in our Privacy Policy.
If you have given your consent for us to set cookies, you can revoke it at any time by clicking on the “Change Cookie Setting” link in the footer of the page.

  • Show details Hide details
    Necessary

    These cookies are necessary to run the core functionalities of this website, e.g. security related functions. With these cookies we can also detect if you want to stay logged into your profile to provide you with fast access to our services after revisiting our website.

    Statistics & Marketing

    In order to continuously improve our website, we anonymously track data for statistical and analytical purposes. With these cookies we can , for example, track the number of visits or the impact of specific pages of our web presence and therefore optimize our content.