Office and administration buildings are equipped with PCs, servers, networks and telecommunication systems. Failure of these systems would bring operation to a standstill since all work processes depend on these systems. Moreover, building automation systems linked via bus systems such as KNX and LON are used in these buildings.
Protection of power supply systems
Combined arresters such as DEHNvenCI and DEHNguard surge arresters can be used to protect power supply systems. DEHNrail , SFL Protector or DEHNsafe protect terminal devices from surges and reduce induced voltages and switching overvoltages to safe values.
Protection of information and telecommunication systems
To ensure safe operation, both data and voice transmission require adequate protection elements. Networks are typically designed in the form of universal cabling systems. Even if fibre optic cables between building and floor distributors are standard today, copper cables are typically installed between the floor distributor and the terminal device. Therefore, the HUBs, bridges or switches must be protected by NET Protector LSA 4TP.
DEHNpatch cables are used to protect terminal devices. The DEHN equipotential bonding enclosure, which can be fitted with LSA disconnection blocks and lightning current carrying DEHNrapid LSA plug-in SPD blocks, can be provided for information technology lines extending beyond the building.
To protect the telecommunication system, NET Protector can be installed in the floor distributor to protect the outgoing lines to the system telephones. A data protection module, for example, can be used for the system telephones.
Protection of building automation systems
Failure of building automation systems can have grave consequences. If the air-conditioning system fails as a result of surges, a data centre may have to be disconnected or a server may have to be shut down.
Bus systems such as KNX / EIB or LON can be protected by BUStector, DEHNconnect or BLITZDUCTOR XT.