AlpTransit Gotthard
The AlpTransit Gotthard tunnel is the most important transit axis for the north–south connection through Switzerland. A reliable power supply is vital in this case.
High-quality arresters from DEHN support the reliable operation of one of the most important transit routes in Europe.

DEHN solution
Internal lightning protection system for the power supply of all ventilation, communication, lighting, and fuse systems in the tunnel
Customer
Alpiq Burkhalter Technik AG (ABAG) | Burkhalter Technics AG, Zürich | Alpiq InTec Ost AG, Spreitenbach | Elektro-Bau AG, Rothrist
Sector
Rail technology
Products
DEHNbloc M 1 255 FM, DEHNguard M TNS 275 FM, DEHNventil M TNS 255 FM
The challenge
A reliable power supply is crucial for the safe operation of the tunnel. We can't afford to have it compromised by lightning currents or surges.
In this system, the entire 50 Hz power supply must be protected. From the main distribution boards to the 176 cross passages.
In view of the high quality requirements, the product decision was made in favour of DEHN's energy-coordinated arresters.

The solution
The protection concept covers the entire power supply.
Components include communication, lighting, control, safety systems such as axle counters and points signals as well as the ETCS (European Train Control System) radio signal. The availability of the power supply protected by DEHN is 99.999996%. This equates to tier 4 classification.
The modular DEHNbloc M arrester with Radax flow spark gap technology protects against partial lightning currents.The associated follow current limitation offers follow current disconnection selectivity even with very small system fuses. Energy coordination with the downstream DEHNguard down conductors is ensured without additional cable lengths. All arresters in the Red/Line family offer a remote signalling output to signal operational readiness to the control centre.
Download reference
DEHN protects the Gotthard railway
AlpTransit Gotthard
More references

Thormählen
Enhancement of the grating fences on the Altmann Bridge in Hamburg with short-circuit wires

TCDD
Reliable operation on the TCDD is ensured, among other things, by a comprehensive lightning and surge protection concept from DEHN.

MVG München
MVG relies on customised lightning and surge protection solutions from DEHN for reliable fire protection in the underground stations.

PINTSCH BAMAG
For the reliable availability of level crossing safety systems, PINTSCH BAMAG relies on DEHN components to protect its railway signalling technology.