RAC spark gap technology

Maximum safety for electrical installations

Know-how from DEHN you can rely on: Rapid Arc Control (RAC) is a state-of-the-art spark gap technology that is used in surge protective devices for power supply systems. Do you need to reliably protect systems from the dangerous consequences of lightning currents and mains follow currents? Then find out more about RAC technology. 

low voltage protection level
high capacity in the shortest possible time
minimal energy input in electrical installations
effective limiting of mains follow currents
Surge arresters without cover with arcing chambers.

What sets the RAC technology apart

01
Unrivalled speed

Speed is safety: The RAC (Rapid Arc Control) spark gap is significantly faster than other spark gap technologies and reduces lightning currents to a level that is safe for the downstream installation. 

02
Minimal residual energy input

The highest energy inputs, even from direct lightning strikes, are safely discharged and only minimal residual energy is transferred to downstream electrical installations – a key advantage compared to commercially available combined arresters with a series connection of varistor and gas discharge tube. 

03
Protects upstream and downstream of the arrester

The RAC technology ensures that upstream fuse devices are subjected only to low loads. Good to know: The DEHNventil M2 series protects terminal equipment at a cable length of up to 10 meters. The costs associated with additional devices and their installation are eliminated. 

This is how the RAC spark gap technology works

The discharge process inside the RAC technology is split into three steps:

Maximum protective effect and efficiency

The internal lightning protection system conducts the lightning current introduced into the installation via the earthing system out of the object to be protected in the best possible way via the mains cable coming from outside. With RAC technology, most of the energy input flows through the RAC spark gap. This preserves connected equipment and systems that can only withstand minimal residual energy for a very short time.

Protection of installations

The RAC technology developed by DEHN significantly reduces the energy input compared to other solutions or technologies. Even with the highest energy inputs, for example from direct lightning strikes. This protects the downstream system and ideally extends its service life. This is possible because the RAC spark gap has a voltage-switching characteristic. This suddenly reduces the surge to a so-called "arc voltage", which is within the range of the nominal voltage.

Efficient arresters

An arrester is maximally efficient if no energy is fed into the installation to be protected and the isolation criteria are fully met. RAC technology comes very close to this ideal situation.
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
2 + 12 =
Solve this simple math problem and enter the result. E.g. for 1+3, enter 4.
This question tests whether you are human or a computer and prevents automated spam submissions.