DEHN Press

Portrait von Ute Pfister vor einem grauem Hintergrund.
Ute Pfister
Spokesperson for Trade Media, Surge Protection in Energy Technology, Lightning Protection/Grounding
+49 151 117 92 610
+49 9181 906-1295
ute.pfister@dehn.de
Portrait von Hannes Wolf vor einem grauem Hintergrund.
Hannes Wolf
Spokesperson for Trade Media, Surge Protection in Information Technology, Safety Equipment, Services
+49 160 31 74 927
+49 9181 906-3303
hannes.wolf@dehn.de
Simon Thaler
Simon Thaler
Director of Corporate Communications
+49 151 146 308 90
+49 9181 906 2339
simon.thaler@dehn.de

Latest posts

Year
Categories
✕

24.11.2025

Image DEHN gala 2025 6708x4472 px
An evening of exceptional performances: DEHN Gala 2025

Employees are the foundation of every successful company. The DEHN Gala once again highlighted just how diverse and varied their contributions can be to a company’s overall success. Last Friday evening, the Neumarkt-based specialist in lightning, surge, and occupational safety invited employees celebrating work anniversaries, graduates of continuing education programs, and, last but not least, the winners of the company’s own Values Awards to its facility in Mühlhausen—for a special evening celebrating special achievements. The highlight of the gala was the recognition of 63 employees for their long-standing service. Four of them can even look back on 45 years at DEHN. When they began their careers at DEHN, the second generation of the DEHN family was still at the helm. Today, Dr. Philipp Dehn, a member of the fourth generation, serves as CEO. The four employees celebrating their anniversaries, who have been part of DEHN since 1980, witnessed how a regional business grew into a globally successful family-owned company. Each of them has made a unique contribution to DEHN’s positive development.Twenty-nine graduates of the training and continuing education programs were also honored—a testament to the company’s efforts beyond its numerous accolades as a training provider. Values That Bring Us TogetherAnother highlight: the presentation of the DEHN Values Awards. Employees from around the world received the award in various categories for their exceptional dedication and exemplary embodiment of the company’s values. 

04.11.2025

Image earth rode set D18014 1200x1200 px
Retrofitting earthing systems: a breeze with the DEHN earth rod set

Retrofitting earthing systems in existing buildings poses challenges for owners and specialised companies. A functioning earthing system is essential, especially when it comes to renovations, energy modernisations or the installation of photovoltaic systems, wall boxes and heat pumps. However, many existing buildings lack proof of standard-compliant earthing or use outdated systems such as water pipe net-works. In addition, limited space, sealed surfaces and difficulty accessing the soil often make conventional retrofitting a complex and costly undertaking. With the new D18014 earth rod set, DEHN provides a practical solution specially developed for the requirements of renovating existing buildings.To comply with standards, the electrical installation must be equipped with a functional earthing system that safely conducts fault currents to earth, thereby ensuring its safety and functionality. It protects people from hazards, such as lightning exposure, and prevents fires. In Germany, an earthing system is a standard requirement for electrical installations, espe-cially in new buildings. But owners of existing buildings often deliberate on whether retrofit-ting is mandatory when they embark on a renovation or modernisation project.Although there is no general obligation to renew the entire electrical installation in older buildings, newly installed or modified system components, such as technical extensions re-lating to renewable energies, must comply with the applicable safety and technical stand-ards. The relevant standards for the installation of an earthing system are DIN VDE AR-N 4100 and DIN 18014.The D18014 earth rod set from DEHN contains all the necessary components for the profes-sional installation of earth rods and is particularly suitable for new buildings and existing buildings with limited soil or minimal excavation possibilities. Whatever the season, the earth rod solution ensures and maintains stable earth resistance regardless of weather con-ditions or soil moisture. The set meets all relevant standards by complying with the re-quirements of DIN 18014 and the applicable VDE specifications. Its versatility makes it suit-able for a variety of applications, including partial renovations, selective upgrades, installa-tion inside the building or a complete renewal of the earthing system.The set consists of five earth rods, each 1 metre long, to be inserted into the ground. A driv-ing spike makes it easier to drive in the rods. The earth rods are connected to the connecting cable (round wire 8-10 mm or cable 16-50 mm2) without a cable lug using a connection clamp. This establishes a secure connection between the earthing system and the main earthing busbar (MEB) of the electrical installation. For buildings with a foundation area of up to 200 m², two sets are required to meet the normative requirements. Installation in-volves minimal disruption of existing outdoor facilities. Only two small excavation sites and wall bushings are necessary.Technical details can be found here. 

27.10.2025

Image DEHNguard md 1500x850 px
Yet more innovation: DEHN opts for new double screw technology for surge protective devices

Long connection cables, which cause inductive voltage drops in switchgear cabinets, often pose a challenge for installers. DEHN solves this problem with an innovative advancement of its proven connection technologies. With the new double screw technology in the Type 2 + 3 surge protective device series DEHNguard MD, the company is once again confirming its pioneering role. This technology complements the existing screw and push-in connection terminal and enables the wiring of different types of conductors. The feed-through wiring option also offers even greater flexibility in terms of electromagnetic compatibility (EMC) for applications with a nominal current of up to 63 A. Push-in technology has proven itself in many areas thanks to its tool-free, fast and secure wiring – especially in residential construction with smaller cross-sections of connection cables. With the new double screw technology, DEHN is now going one step further. Two terminals per pole enable continuous wiring ('V-connection') without additional pin-shaped terminals. The technology allows the use of conductors with a larger cross-section – for two through cables up to 16 mm² each or as a stub line up to 35 mm². This makes it a robust connection that remains permanently stable even under vibration or mechanical stress such as temperature fluctuations.The DEHNguard MD series with double screw technology is particularly advantageous for EMC-compliant wiring in accordance with DIN VDE 0100-534 / IEC 60364-5-53, as there are no high, inductive voltage drops generated across the connection cables. Optional feed-through wiring saves on components and ensures that maximum cable lengths comply with standards. This makes it easier to integrate into existing systems – a huge advantage when retrofitting.The DEHNguard MD has also proven itself in power distribution and switchgear cabinet building, as it meets strict requirements for current-carrying capacity and safety. Areas such as building automation and critical infrastructure also benefit from integrated double screw technology, as it enables durable and low-maintenance connections. In building technology, a supply cable with a cross-section of 16 mm² can now also be easily connected to the device using feed-through wiring.A floating remote signalling contact reliably indicates the status. Defective protection modules in the DEHNguard MD series can be quickly replaced during operation without having to disconnect the wiring.You can find the technical details here.  

15.10.2025

Image Sustainability Report Update EN 1200x1200 px
Making responsibility visible: DEHN update on sustainability

Sustainability is one of the main pillars of DEHN's corporate strategy. In a brief update, the company highlights key figures, progress made, and strategic priorities; thus, providing transparent information on the status of its sustainable development.A little under a year after publishing its first sustainability report, DEHN has produced a revised version for the financial year 2024/2025. This reaffirms the family-owned company's commitment to consistently expanding its responsibility and transparency. Alongside key figures, strategic orientation and organisation, the report highlights the four areas of action: responsible corporate management, being a responsible and attractive employer, responsibility for products and services, and ecological responsibility.Concrete measures, such as determining the “product carbon footprint” (PCF), substantiate this commitment. In 2025, with the aim of assessing and reducing their environmental impact, the PCF was calculated for the first 20 products in the DEHN portfolio. The calculation was carried out in collaboration with the Fraunhofer Institute for Building Physics IBP in line with four internationally recognized standards: ISO 14067, ISO 14040, ISO 14044, and EN 15804+A2. This contribution to climate protection also enables customers to actively improve their own carbon footprint.Moreover, the update focuses on DEHN's progress and continuous pursuit of its sustainability strategy. The ultimate goal is to establish and maintain the right balance between ecological, social and corporate responsibility in the long term.The latest report can be found here.

header_steelclamp_1500x1500px.webp
Hard as steel: The new connection clamp from DEHN

Integrating steel girders, metal sheets, or profiles into lightning protection or equipotential bonding systems often presents a challenge. This is particularly true when protective coatings against corrosion prevent the direct, conductive connection that is essential for effective lightning current discharge or equipotential bonding. The new connection clamp for steel girders from DEHN overcomes this hurdle with a special blade that penetrates coated surfaces up to 0.2 mm without damaging the surface protection. It is therefore particularly suitable for buildings with metallic structures, such as industrial plants, halls, and multi-storey car parks.The clamp is made of high-quality materials and can be used wherever an electrical connection to steel girders, sheets, and profiles is required. With a variable clamping range of 3 to 52 mm, it offers maximum flexibility during installation. The product is approved for use in Zone 2/22 hazardous areas and has a high lightning current carrying capability of up to 100 kA (10/350 μs). It fulfils the requirements of the DIN EN 62561-1 standard and provides a permanently safe, electrically conductive connection even under high loads during a lightning strike.The clamp is available in various designs and materials, both in stainless steel (V2A) and galvanised steel (HDG), with a double clamp or connection bracket. Suitable for round and flat material as well as cables, it is extremely versatile. Typical applications include lightning equipotential bonding with round wire, the installation of air-termination rods without drilling, or the connection of steel girders to earthing systems using connection lugs. The special 7-segment digits also allow use as a test joint, an additional advantage when it comes to testing or maintenance. 

250911_pm_dehn_aunda.jpg
A+A 2025: DEHN sets new standards for electrical safety – comprehensive and smart

Under the slogan 'Vision ZERO: Your path to electrical safety', DEHN will be presenting a broad range of products and solutions for comprehensive work safety at A+A 2025 in Düsseldorf. From 4 to 7 November, DEHN will be demonstrating how innovative solutions, digital services and practical applications can ensure greater safety in the workplace at stand B59 in hall 14. DEHN takes its holistic approach to protection based on the 'TOP principle', which encompasses technical, organisational, and personal measures one step further by integrating smart technology. The expert for safety equipment offers tailor-made solutions for each of these areas, which can be flexibly integrated into different safety concepts. DEHN is thus expanding the approach to ‘TOP+S’.The DEHNshort arc fault protection system supports technical safety by being integrated into low-voltage installations. It detects electric arcs and stops them within milliseconds. This significantly reduces the incident energy and enables rapid recommissioning. The DEHNproX product range from DEHN includes safety devices for implementing the 5 safety rules and live working. This year, the company is introducing a new smart highlight from this product series. DEHNarX carries out systematic risk assessments and defines targeted protective measures. This service is provided by arc fault protection experts at DEHN. In addition, DEHNcare personal protective equipment not only provides reliable protection in the event of an arc fault, but also impresses due to being very comfortable to wear and available in a wide range of sizes for men and women. The DEHNsense EFD (Electrical Field Detector) complements the TOP principle as a smart, technical measure. The small, compact device, which can be easily worn on a helmet or wrist, detects electrical hazards at an early stage, warns immediately upon entering the danger zone and thus increases safety when working on electrical systems. The EFD can be individually configured using the DEHNwork app. Depending on the requirements of the respective system, the device can be conveniently adjusted via smartphone.With its combination of electrical engineering expertise, smart technologies and practical solutions, DEHN is setting new standards for electrical safety – comprehensive, digital and smart. Experience safety – with structure and strategyA special highlight of this year's A+A trade fair appearance is the interactive tour of the exhibition stand into the world of electrical safety. He guides visitors through the various protection levels and brings DEHN's protection solutions to life in a practical way.

09.09.2025

Image Team EcoVadis 2560 x 1440 px
Holistic approach to sustainable business: EcoVadis honours DEHN for its commitment to sustainability

As of August 2025, DEHN SE ranks among the top 15 percent of companies assessed by EcoVadis. This is confirmed by the silver medal awarded by the leading provider of global sustainability ratings. ‘We are very proud that our efforts have been acknowledged with the silver medal. For us, this is a big step in the right direction and an incentive for further successes in the area of sustainability,’ explains Dr Philipp Dehn, CEO of DEHN SE.EcoVadis' rating method is based on international sustainability standards such as the Global Reporting Initiative (GRI), the UN Global Compact and ISO 26000. The platform enables companies to assess the sustainability performance of their suppliers worldwide.The assessment focuses on four areas: environment, labour and human rights, ethics and sustainable procurement.The specialist for lightning and surge protection and safety equipment operates photovoltaic systems with a capacity of 1,250 kWp for its own electricity generation at its Mühlhausen site. Energy is saved through heat recovery and concrete core activation. The new production facility also complies with the KfW 40 standard and has extensive environmentally friendly green roofing and areas with typical local sandy grassland. The company already uses only green electricity at its headquarters in Neumarkt.In its supply chain, DEHN relies on transparent processes and a partnership-based approach to suppliers. DEHN has been part of the UN Global Compact since 2024, a commitment underlined by its own code of conduct for business partners and comprehensive risk management in accordance with the Supply Chain Due Diligence Act (LkSG).DEHN develops durable products and supplements them with digital services to conserve resources and increase safety in an increasingly electrified world. Anchoring sustainability firmly in product design and innovation processes is a goal the company is striving hard to achieve.As an employer, DEHN also demonstrates responsibility by offering professional development opportunities, flexible working hours for a good work-life balance, and a wide range of health care options. The same applies to active inclusion, for example, through cooperation with the JURA Werkstätten in Neumarkt to integrate people with disabilities into the workplace at the site in Mühlhausen. ‘With the EcoVadis rating, we want to make it clear to our customers and suppliers that sustainability is not only an important value in our partnership but, alongside innovation, a cornerstone of our success,’ explains Susanne Horn, Director of Corporate Development at DEHN.

27.06.2025

250627_pr_dehn_weltblitzschutztag.jpg
World Lightning Safety Day 2025: Safety Starts Before the Lightning Strikes

The German Insurance Association (GDV) estimates that lightning and surge damage will cost 350 million euros in 2024. 1.5 million of the 100 million lightning strikes worldwide were recorded in Germany. This trend underscores the importance of reliable protection solutions. As a specialist in lightning, surge, and occupational safety, DEHN is committed to protecting people, buildings, and technical systems, and is highlighting the importance of this issue, particularly on this year’s World Lightning Protection Day. These days, there is an increase in thunderstorms again. Especially in the summer, thunderstorms occur more frequently and increase the risk of lightning strikes. Modern households are equipped with numerous sensitive electronic devices that can easily be damaged by surges. These include smart home technology, photovoltaic systems, charging stations, and heat pumps. Effective lightning and surge protection can not only safeguard electronics from destruction but also prevent fires caused by lightning strikes. Especially since damage caused by power surges is not always covered by home contents or building insurance. A good reason to take appropriate measures for lightning and surge protection in your home. DEHN offers comprehensive protection solutions—from consultation to implementation As a reliable partner, DEHN supports customers with comprehensive solutions for external and internal lightning protection—from air-termination systems and grounding systems to surge protection devices. External lightning protection safely diverts lightning strikes into the ground and protects buildings from fire. Internal lightning protection prevents damage to electrical systems and equipment. Whether for private homes, commercial buildings, critical infrastructure, hospitals, data centers, or energy suppliers—reliable lightning and surge protection is indispensable in all sectors. For over 115 years, DEHN has stood for protection, quality, and innovation. In addition to a broad product portfolio, the company offers customized protection concepts. You can find a clear overview of our specific solutions, including product recommendations, documentation, and helpful services, on our website.

18.06.2025

Image Romania 1200x1200px
Greater manufacturing capacity for European markets: DEHN breaks ground for production in Romania

Global electrification is the main driver of business for the family-owned company DEHN. The expansion of renewable energies, the growing share of electric vehicles, the necessary infrastructure, data centres and much more require products and solutions from the specialist for lightning protection, surge protection and safety equipment. The new production site in Piteşti, Romania, expands capacities for customers in Europe. The plant fits seamlessly into the company's existing global production network. "Piteşti gives us the flexibility we need to supply our customers in Europe even better," says Dr Philipp Dehn, CEO DEHN SE. "The plant underscores our internationalisation efforts and creates future-proof jobs in the greater Bucharest area."Open configuration optionsTo meet the anticipated global market demand, the company recently opened additional production sites in Mühlhausen  (Germany) and  Mooresville (North Carolina, USA). As the existing capacities in Germany will soon reach their limits, DEHN is now pushing ahead with the construction of an additional production facility for the European markets. After an intensive search for a location, during which several cities and regions throughout Europe were evaluated, the decision fell in favour of Piteşti, located north-west of the Romanian capital Bucharest. The combination of a well-trained workforce, very good local conditions and sufficient space for the construction project were the key arguments in favour of the new site in the CTPark Piteşti. DEHN plans to invest around 10 million euros in this Eastern European plant over the coming years. While the production sites in Neumarkt and Mühlhausen will primarily focus on high-volume products and highly automated processes in future, the focus in Romania will be on customised surge protection products in smaller quantities that require a high level of manual production.The ground-breaking ceremony marks the start of an approximately 10-month construction phase. Start of production with up to 150 employees is scheduled for mid-2026.

19.03.2025

Image DEHN joins the odca 1500x850px
DEHN joins the Open Direct Current Alliance

DC technology plays a key role in the modern energy landscape. Whether photovoltaics, battery storage systems or charging stations, DEHN has been dealing with the protection of DC systems for a long time. DEHN's involvement in the Open Direct Current Alliance therefore marks a further milestone in the lightning and surge protection specialist's endeavour to shape the future of the electrical industry with innovative and sustainable solutions. DEHN has already successfully participated in the DC-INDUSTRIE research project, which investigated the advantages and potential of DC technologies in industrial applications.‘Our membership of the Open DC Alliance once again symbolises our commitment to promoting sustainable and innovative energy solutions,’ said Christian Höhler, CTO of DEHN SE. ‘We look forward to being at the forefront of DC technology, alongside other industry leaders, and actively shaping the future of energy supply.’The Open DC Alliance is a leading consortium dedicated to promoting and standardising DC technologies. As a member of the Alliance, DEHN can contribute to the development and implementation of future-oriented DC solutions that improve the efficiency and environmental impact of the energy supply. DC technologies offer significant environmental benefits. They reduce energy losses and increase energy efficiency which, in turn, reduces CO₂ emissions and allows a more sustainable use of resources.Renewable energies, like photovoltaic systems, and storage systems, such as fuel cells, can be integrated much more efficiently into a DC grid. That is why direct current is an essential component for the success of the energy transition. The two DC INDUSTRIE research projects reveal that energy consumption in existing systems can be reduced by up to ten per cent. Another benefit is the reduced need for copper in conductors. While conductors with four to five wires are required for alternating voltage, one to two wires less are needed for direct voltage. This represents a copper saving of more than 40 per cent.For many years, DEHN has been committed to protecting DC systems and offers customised protection solutions. The company has a DC test field where surges and DC networks can be simulated. The specific source characteristics of PV systems can also be reproduced there.The company was particularly active in the forerunner project DC-INDUSTRIE and was able to gain valuable insights and experience.   These are channelled into pilot projects dealing with DC grids in industrial applications and buildings. DEHN supplies, for example, DC surge arresters for local public transport systems and special surge protection solutions for photovoltaic systems.Further information on DEHN’s DC range or sustainability efforts (sustainability | DEHN) can be found on our website DEHN - lightning protection, surge protection, safety equipment.