Service specifications DEHNconcept

Calculation of earth-termination systems of transformer substations

Basic principle

DIN EN 50522 (VDE 0101-2):2011-11 part 2 in the version valid at the time of placing the order;
DIN VDE 0100 part 410, part 540 in the version valid at the time of placing the order;
DIN VDE 0185-305-3 in the version valid at the time of placing the order;
DIN 18014 in the version valid at the time of placing the order;
DIN VDE 0151 in the version valid at the time of placing the order;
DIN VDE 0141 in the version valid at the time of placing the order;

(Should at the time of placing the order any of the above-mentioned standards be in a period of transition between two versions, the latest version shall apply.)
(In the case of IEC standards, there is no transition period between two versions.)

Prerequisites

  1. Basic information on the electrical installation (DEHN data sheet)
  2. Construction of transformer, e.g. solid earthing / isolated neutral
  3. Optional: fee-based site survey / project meeting

Service description

  1. Result of the calculation of the conductor cross-section depending on the material
  2. Technical parameters of the electrical installation using a DEHN calculation programme

Scope of service

  1. Calculation of the interior earthing in the station room
  2. Calculation of the protective conductor to the MEB
  3. Calculation of the MEB
  4. Calculation of the earthing and short-circuiting device (at primary terminals)
  5. Calculation of the earthing and short-circuiting device (at secondary terminals)
  6. General description (PDF document)

Document format

  • All documents will be handed over electronically in PDF format.
  • Documents can be provided in open format (e.g. .docx, .xlsx) if a separate handover document is signed to this effect.

Creation of CAD drawings of structures for designing lightning protection systems

Basic principle

For designing lightning protection systems and the protected volume of the air-termination systems, the current building stock must be displayed to scale in a CAD file. If neither 2D nor 3D CAD files are available when ordering the design of a lightning protection system, they can be redrawn based on existing paper drawings and / or pixel scans of as-completed drawings (2D or 3D drawings).

Prerequisites

  1. Drawings of the building / installation to be protected in non-editable electronic format or paper form
  2. Optional: a fee-based site survey / project meeting

Service description

Drawing of the building / installation to be protected (2D or 3D CAD files)

Scope of service

Drawing of the outer shell of the building / installation to be protected which is required for planning a lightning protection system (2D or 3D CAD files)

Document format

  • All documents related to the service are supplied electronically in PDF format.
  • Open formats (z. B. .docx, .xlsx, .dwg, .dxf) require prior signature of a separate document.

Design of a surge protection concept

Basic principle

DIN EN 62305-3 (VDE 0185-305-3) in the version valid at the time of placing the order;
DIN EN 62305-4 (VDE 0185-305-4) in the version valid at the time of placing the order;
DIN VDE 0100-443 (VDE 0100-443) in the version valid at the time of placing the order;
DIN VDE 0100-534 (VDE 0100-534) in the version valid at the time of placing the order;
DIN VDE 0100-712 (VDE 0100-712) in the version valid at the time of placing the order;

(Should at the time of placing the order any of the above-mentioned standards be in a period of transition between two versions, the latest version will apply.)

Optional:
IEC 62305-3 in the version valid at the time of placing the order;
IEC 62305-4 in the version valid at the time of placing the order;
IEC 60364-4-44 in the version valid at the time of placing the order;
IEC 60364-5-53 in the version valid at the time of placing the order;
IEC 60364-7-712 in the version valid at the time of placing the order;

(In the case of IEC standards, there is no transition period between two versions)

Prerequisites

  1. Basic information on the electrical installation
  2. Provision of flow charts for the electrical installation
  3. Optional: a fee-based site survey / project meeting (Part No. S03070)

Service description

Selection of surge protective devices with the help of the DEHNselect SPD selection software in the DEHNsupport Toolbox or via conventional selection means

Scope of service

  1. Flow chart of electrical installation including relevant parts lists for the required surge protective devices (without any accessories which may be necessary, e.g. additional arrester backup fuses)
  2. Optional: Preparation of a tender specification
  3. Optional: Provision of product data sheets and installation instructions

Document format

  • All documents in the scope of service will be handed over electronically in PDF format.
  • Documents can be provided in open format (e.g. .docx, .xlsx) if a separate handover document is signed to this effect.

Lightning protection risk management

Basic principle

Version of DIN EN 62305-2 (VDE 0185-305-2) applicable when placing the order;

(If the above standard has a transition period, the more recent version shall apply.)

Alternative:
Version of IEC 62305-2 applicable when placing the order;

(There is no transition period between IEC standards.)

Prerequisites

  1. Fully completed and signed questionnaire for assessing the risk for structures and additional documents (e.g. fire protection document)
  2. Optional: Fee-based on-site survey / project meeting  to answer the questionnaire for assessing the risk for structures together with the customer

Service description

Risk management according to DIN EN 62305-2 or IEC 62305-2 based on the input parameters given by the customers or generated together with the customer

Scope of service

  1. Definition of the relevant structure and its properties
  2. Definition of all types of loss for the relevant structure and the associated risks R1, R2, R3 and R4
  3. Assessment of the risk for each type of loss selected
  4. Assessment of the need for protection by comparing the selected risks (R1, R2 and R3) for a structure with the tolerable risk RT
  5. When selecting R4: Assessment of the economic efficiency of the protection measures by comparing the costs of a total loss with and without protection measures

Document format

  • All documents related to the service are supplied electronically in PDF format.

  • Open formats (e.g. .docx, .dsprj) require prior signature of a separate document.

Travel expenses for site survey / project meeting

Basic principle

If the documentation for a building requiring lightning protection measures is non-existent or incomplete, it is wise for the planner to conduct a site survey as the basis for planning the lightning protection system, including the air-termination system and its protected volume. A face-to face meeting with the client provides the opportunity to elicit his expectations concerning the planning of lightning protection measures and explain possible solutions.

Prerequisites

  1. The client’s decision maker must participate in the meeting
  2. Accessibility of the site to be inspected
  3. Permission to take photographs
  4. Information about the personal protective equipment required

Service description

  1. Site survey of plant/facility
  2. Discussion of fundamental solutions

Scope of service

  1. Site survey of plant/facility
  2. Photographic documentation of the plant/facility
  3. Determination of possible lightning protection solutions

Document format

All documents in the scope of service will be handed over electronically in PDF format.

Calculation of the separation distance

Basic principle

Version of DIN EN 62305-3 (VDE 0185-305-3) applicable when placing the order;

(If the above standard has a transition period, the more recent version shall apply.)

Alternative:
Version of IEC 62305-3 applicable when placing the order;

(There is no transition period between IEC standards.)

Prerequisites

  1. Electronic drawings of the lightning protection system of the building / installation to be protected must be provided in the following data formats:

  • 2D: .dxf, .dwg, .pdf
  • 3D: .dwg, .skp, .pdf

2.  Optional: a fee-based site survey / project meeting

Service description

Calculation of the separation distance according to subclause 6.3 of DIN EN 62305-3 or IEC 62305-3

Scope of service

  1. Description of the calculation of the separation distance including explanation of the solution approaches and boundary conditions which may have to be observed
  2. Drawing including the necessary separation distances from the DEHNsupport Distance Tool

Document format

  • All documents related to the service are supplied electronically in PDF format.

  • Open formats (e.g. .docx, .pri) require prior signature of a separate document.

Surveillance of the installation of lightning protection systems

Basic principle

Correct installation of lightning protection systems as planned based on product-specific installation requirements for the lightning protection components used requires surveillance and documentation of the installation process. This allows to detect installation errors and initiate their elimination.

Prerequisites

Design services performed

or

or

and / or

Service description

  1. Coordination between the principal and the contractor at the construction site
  2. Precise adaptation of the above mentioned design services to the local conditions
  3. Preparation of a surveillance documentation (daily construction records) including photos and comments

Scope of service

  1. Daily construction records including photos and description of the installation performed
  2. Precise adaptation of the design documents (drawings, bills of material) to the actual installation of the lightning protection system

Document format

  • All documents related to the service are supplied electronically in PDF format.

  • Open formats (e.g. .docx, .xlsx, .dwg, .dxf) require prior signature of a separate document.

Checking whether the lightning protection system installed corresponds to the design documents

Basic principle

Correct installation of lightning protection systems as planned based on product-specific installation requirements for the lightning protection components used (decisive for the proper operation of the lightning protection system). Checking whether the lightning protection system installed corresponds to the design documents is a necessary prerequisite for testing and maintaining the lightning protection system.

Prerequisites

Design services performed

or

or

and / or

Service description

  1. Comparison of the design documents with the lightning protection system installed on site
  2. Documentation including photos and comments

Scope of service

Documentation including photos and comments

Document format

  • All documents related to the service are supplied electronically in PDF format.

  • Open formats (e.g. .docx, .xlsx, .dwg, .dxf) require prior signature of a separate document.

General

Checking whether the lightning protection system installed corresponds to the design documents does not replace the requirements for maintaining and testing a lightning protection system according to section 7 of the IEC/EN 62305-3 standard valid when placing the order.

Design of external lightning protection systems (without earth-termination systems) with isolated air-termination systems and down conductors

Basic principle

Version of DIN EN 62305-3 (VDE 0185-305-3) applicable when placing the order;

(If the above standard has a transition period, the more recent version shall apply.)

Alternative:
Version of IEC 62305-3 applicable when placing the order;

(There is no transition period between IEC standards.)

Prerequisites

  1. Project data sheet must be fully completed (form provided by DEHN+SÖHNE)
  2. Electronic drawings of the building / installation to be protected must be provided in one of the following data formats:
  • 2D: .dxf, .dwg
  • 3D: .dwg, .skp, dgn, stp
  • Optional: Fee-based generation of drawings or fee-based 3D scan for generating 3D data of the building / installation to be protected

3.  Optional: a fee-based site survey / project meeting

Service description

  1. Dimensioning of the air-termination systems of the lightning protection system (LPS) according to the selected class of LPS using the rolling sphere method in line with subclause 5.3.3 of DIN EN 62305-3 or IEC 62305-3 taking account of the wind loads according to EUROCODE 1
  2. Dimensioning of the down conductors of the lightning protection system (LPS) according to the selected class of LPS
  3. Drawings of the air-termination systems and down conductors of the building / installation to be protected
  4. Design of the protected volume of the air-termination systems (2D or 3D depending on the provided data format of the building / installation to be protected)
  5. Preparation of a bill of material of the lightning protection components
  6. Calculation of the separation distance according to subclause 6.3 of DIN EN 62305-3 or IEC 62305-3
  7. Optional: Fee-based design of the earth-termination system for external lightning protection systems
  8. Optional: Fee-based planning of surge protection measures

Scope of service

  1. Description of the lightning protection concept / lightning protection solution including explanation of the solution principles and boundary conditions which may have to be observed for design
  2. Drawings of the roof view and protected volumes (2D or 3D depending on the provided data format of the building / installation to be protected)
  3. Drawings of the mounting details of the lightning protection components used
  4. Bill of material (including material quotation in case of customer conditions for lightning protection material)
  5. Product data sheets, manufacturer’s declarations and installation instructions (if any) of the components used for design
  6. Optional: Free tender specifications of the components used for design

Document format

  • All documents related to the service are supplied electronically in PDF format.

  • Open formats (e.g. .docx, .xlsx, .dwg, .dxf) require prior signature of a separate document.

Design of external lightning protection systems (without earth-termination systems) with non-isolated air-termination systems and down conductors

Basic principle

Version of DIN EN 62305-3 (VDE 0185-305-3) applicable when placing the order;

(If the above standard has a transition period, the more recent version shall apply.)

Alternative:
Version of IEC 62305-3 applicable when placing the order;

(There is no transition period between IEC standards.)

Prerequisites

  1. Project data sheet must be fully completed (form provided by DEHN+SÖHNE)
  2. Electronic drawings of the building / installation to be protected must be provided in one of the following data formats:
  • 2D: .dxf, .dwg
  • 3D: .dwg, .skp, dgn, stp
  • Optional: Fee-based generation of drawings or fee-based 3D scan for generating 3D data of the building / installation to be protected

3.  Optional: a fee-based site survey / project meeting

Service description

  1. Dimensioning of the air-termination systems of the lightning protection system (LPS) according to the selected class of LPS using the rolling sphere method in line with subclause 5.3.3 of DIN EN 62305-3 or IEC 62305-3 taking account of the wind loads according to EUROCODE 1
  2. Dimensioning of the down conductors of the lightning protection system (LPS) according to the selected class of LPS
  3. Drawings of the air-termination systems and down conductors of the building / installation to be protected
  4. Design of the protected volume of the air-termination systems (2D or 3D depending on the provided data format of the building / installation to be protected)
  5. Preparation of a bill of material of the lightning protection components
  6. Calculation of the separation distance according to subclause 6.3 of DIN EN 62305-3 or IEC 62305-3
  7. Optional: Fee-based design of the earth-termination system for external lightning protection systems
  8. Optional: Fee-based planning of surge protection measures

Scope of service

  1. Description of the lightning protection concept / lightning protection solution including explanation of the solution principles and boundary conditions which may have to be observed for design
  2. Drawings of the roof view and protected volumes (2D or 3D depending on the provided data format of the building / installation to be protected)
  3. Drawings of the mounting details of the lightning protection components used
  4. Bill of material (including material quotation in case of customer conditions for lightning protection material)
  5. Product data sheets, manufacturer’s declarations and installation instructions (if any) of the components used for design
  6. Optional: Free tender specifications of the components used for design

Document format

  • All documents related to the service are supplied electronically in PDF format.

  • Open formats (e.g. .docx, .xlsx, .dwg, .dxf) require prior signature of a separate document.

Design of external lightning protection systems (without earth-termination systems) with isolated and non-isolated air-termination systems and down conductors

Basic principle

Version of DIN EN 62305-3 (VDE 0185-305-3) applicable when placing the order;

(If the above standard has a transition period, the more recent version shall apply.)

Alternative:
Version of IEC 62305-3 applicable when placing the order;

(There is no transition period between IEC standards.)

Prerequisites

  1. Project data sheet must be fully completed (form provided by DEHN+SÖHNE)
  2. Electronic drawings of the building / installation to be protected must be provided in one of the following data formats:
  • 2D: .dxf, .dwg
  • 3D: .dwg, .skp, dgn, stp
  • Optional: Fee-based generation of drawings or fee-based 3D scan for generating 3D data of the building / installation to be protected

3.  Optional: a fee-based site survey / project meeting

Service description

  1. Dimensioning of the air-termination systems of the lightning protection system (LPS) according to the selected class of LPS using the rolling sphere method in line with subclause 5.3.3 of DIN EN 62305-3 or IEC 62305-3 taking account of the wind loads according to EUROCODE 1
  2. Dimensioning of the down conductors of the lightning protection system (LPS) according to the selected class of LPS
  3. Drawings of the air-termination systems and down conductors of the building / installation to be protected
  4. Design of the protected volume of the air-termination systems (2D or 3D depending on the provided data format of the building / installation to be protected)
  5. Preparation of a bill of material of the lightning protection components
  6. Calculation of the separation distance according to subclause 6.3 of DIN EN 62305-3 or IEC 62305-3
  7. Optional: Fee-based design of the earth-termination system for external lightning protection systems
  8. Optional: Fee-based planning of surge protection measures

Scope of service

  1. Description of the lightning protection concept / lightning protection solution including explanation of the solution principles and boundary conditions which may have to be observed for design
  2. Drawings of the roof view and protected volumes (2D or 3D depending on the provided data format of the building / installation to be protected)
  3. Drawings of the mounting details of the lightning protection components used
  4. Bill of material (including material quotation in case of customer conditions for lightning protection material)
  5. Product data sheets, manufacturer’s declarations and installation instructions (if any) of the components used for design
  6. Optional: Free tender specifications of the components used for design

Document format

  • All documents related to the service are supplied electronically in PDF format.

  • Open formats (e.g. .docx, .xlsx, .dwg, .dxf) require prior signature of a separate document.

Design of earth-termination systems for external lightning protection systems

Basic principle

Version of EN 62305-3 applicable when placing the order;
Version of DIN 18014 applicable when placing the order;

(If the above standards have a transition period, the more recent version shall apply.)

Alternative:
Version of IEC 62305-3 applicable when placing the order;

(There is no transition period between IEC standards.)

Prerequisites

  1. Drawings of the building / installation to be protected in electronic form in the following data formats:
  • 2D: .dxf, .dwg
  • 3D: .dwg, .skp
  • Optional: Fee-based order of creation of drawings

2.  Optional: a fee-based site survey / project meeting

Service description

  1. Dimensioning of the earth-termination system of the lightning protection system (LPS) in conformity with the class of LPS selected according to sub-clause 5.4 of EN 62305-3 or IEC 62305-3 and DIN 18014
  2. Drawing of the earth-termination system on and/or in the building / installation to be protected
  3. Preparation of a bill of materials of the components for the earth-termination system

Scope of service

  1. Description of the earthing concept / earth-termination system including explanation of the solution principles and boundary conditions which may have to be observed for the practical implementation of the design
  2. Drawings of the earth-termination system
  3. Drawings of the mounting details for the lightning protection components used
  4. Bill of materials (including material quotation in case of customer conditions for lightning protection material)
  5. Product data sheets, manufacturer’s declarations and installation instructions (if any) of the components used for design
  6. Optional: Free tender specifications of the components used for design

Document format

  • All documents related to the service are supplied electronically in PDF format.

  • Open formats (e.g. .docx, .xlsx, .dwg, .dxf) require prior signature of a separate document.
返回顶部