IPI intelligent transformer substations by Ingenieurbüro Pfeffer
Pfeffer relies on a tested lightning and surge protection concept from DEHN to ensure security of supply as well as system and operational safety and to fulfil normative requirements, e.g. pursuant to DIN VDE 0100-443.

DEHN solution
Protection concept for intelligent transformer substations
Customer
Ingenieurbüro Pfeffer GmbH
Sector
Energy
Products
DEHNvenCI, DEHNrail, Blitzductor XT, DEHNpatch, DEHNgate
The challenge
The intelligent expansion of the power supply network, integration of renewable energy sources and electromobility, all present the power supply companies with new challenges. This applies in particular to the field of transformer substations.
The construction of new and expensive power lines can be optimised using intelligent transformer substations. In doing so, the IPI ION acts as an outpost of the control room. The implementation of intelligent solutions like adjustable transformer substations, longitudinal voltage regulators, control systems and telecontrols as well as monitoring units serves the timely detection of grid overloads, the reduction or prevention of power failures and enables quick and preventative troubleshooting. Constant availability is essential here.
As, however, the secondary technology installed consists of sensitive electronic components and there is an increased risk of injecting lightning current and surges from nearby and distant lightning strikes in the increasingly networked smart grid, the risk of damage is growing.
The consequence is expensive repair and maintenance work involving considerable manpower and reducing availability.
The solution
Pfeffer relies on a tested lightning and surge protection concept from DEHN to ensure security of supply as well as system and operational safety and to fulfil normative requirements, e.g. pursuant to DIN VDE 0100-443.
To protect the power side, a DEHNvenCI is installed directly at the feeding point of the low-voltage side in accordance with DIN VDE 0100-534. This is a combined arrester Type 1+2+3 based on spark-gap technology. Thanks to the integrated arrester backup fuse, it can be installed in a space-saving and practical manner regardless of the nominal current of the system.
In addition, copper-based information and communication lines are protected with the BLITZDUCTOR-XT or DEHNpatch. The same applies to coaxial cables leading to external transmission technology. Here, DEHNgate provides reliable protection against the field effects of lightning. Depending on the system configuration, sensitive control devices are also protected with Type 3 surge arresters such as DEHNrail.
There is also the option of integrating the surge protection devices into the control room so that a preventive maintenance concept can be realised.
Download reference
Ingenieurbüro Pfeffer
Protection concept for intelligent transformer substations
More references

Langmatz
In the street lighting sector, many local authorities and municipal utilities are converting to LED technology.

Bender
Power quality measuring equipment must also function reliably in the event of surges. Bender relies on a professional solution from DEHN to protect its power quality analysers.

INSYS
To minimise unscheduled downtimes of systems and machines, INSYS relies on a professional protection solution from DEHN for its predictive maintenance concept.

INTILION
INTILION has opted for a comprehensive protection concept from DEHN to ensure the permanent and secure availability of its battery storage systems.

Netze BW GmbH
DEHN protects digital measurement technology for the smart grid in low-voltage systems.

VARTA Storage GmbH
VARTA has opted for a comprehensive protection concept from DEHN to ensure the permanent and secure availability of its container battery storage systems.

IDS GmbH
IDS GmbH relies on a comprehensive solution from DEHN for the lightning and surge protection of its compact ACOS 730 small telecontrol device.

WAGO telecontrol solutions
DEHN protects WAGO telecontrol solutions for monitoring power grids against damage caused by lightning and surges.

FEST
DEHNconcept planning service for hydrogen electrolysis systems of the FEST Group.