Surge protection for wall boxes

Whether it's in your own garage, at work or at the supermarket: wallboxes are welcome. Not only do they make a substantial contribution to the expansion of the charging infrastructure, they also take up little space and blend discreetly into the appearance of the building. It is therefore all the more important to protect their permanent availability and enable uninterrupted charging. Overvoltages in particular, for example caused by lightning strikes in the vicinity, pose a risk to the function of the wallbox and the connected vehicle. Standards such as IEC 60364-4-44, section -443, and IEC 60364-5-54, section -534, therefore regulate the use of overvoltage protection measures.

Due to the compact design of wallboxes, the installation of protective devices is often challenging and complicated in practice – for manufacturers of charging equipment as well as for planning engineers and installers. The solution? Our compact surge arresters, specially developed for confined installation situations. Find out here what you need to consider when integrating standard-compliant surge protection and how our solutions can be installed even in the smallest of spaces.

Wallbox surge protection by DEHN

Securing buildings with wallboxes in compliance with standards

In principle, IEC 60364-4-44, section -443, requires surge protection in residential buildings. This includes the Wall box. Protection measures must be taken in the main distribution board and as close as possible to the feeding point. IEC 60364-5-54, section -534 specifies which overvoltage protection you require and how it is to be installed. Among other things, it stipulates that for cable lengths of up to 10 metres to the building's main distribution board, the wallbox is located within the protected range. If the cable lengths exceed the requirement of 10 metres, the wallbox and therefore also the electric vehicle are outside the protected area. In this case, you should take further protective measures for the power and data lines in the charging circuit.

Safely standard-compliant

Our solutions and products are standard-compliant. Learn more about the requirements and how you can meet them with our solutions.
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
3 + 0 =
Solve this simple math problem and enter the result. E.g. for 1+3, enter 4.
This question tests whether you are human or a computer and prevents automated spam submissions.