The 5 safety rules of electrical engineering

Working in and around electrical installations can be life-threatening. That is why there are five safety rules that every electrician should know and follow. Whether testing electrical systems or carrying out installation and maintenance work: the five safety rules set out a clear procedure for working in disconnected areas or in the vicinity of live areas. Your compliance protects human life. 

DEHN

This is where the 5 safety rules come into play

The five safety rules for handling electrical energy are applied across various sectors, whether in the field of distribution network operators, industry, power suppliers, photovoltaics, rail, e-mobility and more. Put simply: wherever energy is generated, consumed or distributed, you will also encounter life-saving measures. 

The exact areas of the installation that fall under the compliance obligation and what other protective measures need to be taken are determined in the course of the risk assessment.  

Enable your employees to apply the five safety rules correctly and ensure that they are reliably protected. We will support you with our products, our services and our expertise. 

These are the 5 safety rules

DEHN
1. Disconnect completely

Disconnection means the electrical installation is disconnected from live parts on all poles. 

DEHN
2. Secure against reconnection

Prevent the accidental activation of the system. Re-powering must be reliably prevented. In the low-voltage system, this is preferably done by blocking the actuating mechanism – or you can replace the unscrewed fuses with lockable blocking elements.

DEHN
3. Verify that the installation is dead

Verifying that the installation is dead is performed with a voltage detector. Ensure in advance that the selected voltage detector is suitable for the expected operating voltage, frequency and ambient conditions and check the voltage detector is working correctly. In addition, make sure that voltage detectors for high voltage have been periodically tested. When using a contact voltage tester, uninsulated parts must be contacted in order to establish a reliable electrical contact and to verify the absence of voltage. 

DEHN
4. Earthing and short-circuiting

Important: First earth, then short circuit! 
If the system is dead, first connect the earthing and short-circuiting devices (EaS) to the earthing system and then connect them to the parts to be earthed. Disassembly occurs in reverse order to the above. If possible, the earthing and short-circuiting devices must be visible from the work location. Otherwise, they should be placed as close to the work location as possible. 

DEHN
5. Provide protection against adjacent live parts 

According to the five safety rules, adjacent parts are parts located in the vicinity zone. 

If there are parts of the system near the work location that cannot be disconnected, you must take additional safety measures before starting work. In this case, use insulating protective shutters or insulating cloths, for example, to protect against accidental contact with live parts. 

Safely standard-compliant

Our solutions and products are standard-compliant and meet the requirements of the standard DIN EN 50110-1 that applies across Europe. 

Our services

We provide you with a wide range of services that meet the requirements of the five safety rules. This will give you an overview. 
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
2 + 2 =
Solve this simple math problem and enter the result. E.g. for 1+3, enter 4.
This question tests whether you are human or a computer and prevents automated spam submissions.