Surge protection with ACI technology: knowledge for planning engineers and experts

Technical background on ACI technology, TOVs, selectivity, cable routing and SPD installation.

From TOVs and broken neutral conductors to selectivity and choosing the right type of SPD: this page brings together technical background information, expert answers to frequently asked questions and in-depth information on modern surge protection using DEHN's ACI technology. 

  • ACI technology 
  • TOVs & broken neutral conductors 
  • Selectivity 
  • Type 1–3 SPDs 
ACI-Technologie
TOV / Netzstabilität
Planung & Installation
OD

Surge protection does not end with the selection of an SPD. Cable routing, selectivity and behaviour in the event of a fault are also crucial.  

Oliver Dumhard
Product Manager

Key questions at a glance

When are Type 1–3 arresters used?

Type 1 SPDs are typically installed at the feeding point of the system. They are essential for structures with external lightning protection or power supply via overhead lines. They are designed to safely divert the high currents caused by a direct lightning strike. The most important parameter is the lightning impulse current (Iimp), which must be at least 12.5 kA for class of LPS III/IV and at least 25 kA per path for class of LPS I/II. 

Type 2 SPDs are typically installed in the sub-distribution boards of a system. They protect against overvoltages caused by switching operations in the grid or indirect lightning strikes. The nominal discharge current (In) must be at least equal to the values specified in DIN VDE 0100-534 (e.g. 5 kA or 20 kA). 

Type 3 SPDs are installed close to the equipment to provide direct protection for sensitive terminal devices. They complement Type 1 and Type 2 SPDs and form the final stage of protection in the surge protection concept. 

 

What does TOV stand for?

TOV stands for temporary overvoltages and refers to temporary power-frequency overvoltages. They can be caused by a broken neutral conductor. TOVs are power-frequency overvoltages that persist for extended periods.  

In conventional Type 2 surge arresters, a broken neutral conductor causes the internal disconnector to disconnect the SPD from the mains. In contrast, Type 2 arresters featuring ACI technology can withstand this fault condition and remain safely connected to the mains.

Why do TOVs pose a challenge for SPDs?

TOVs almost always result in the SPD being disconnected, interrupting the system's protection. If any overvoltage events occur before the SPD is replaced, the system will no longer be protected.  

How do conventional SPDs behave during TOVs?

Conventional standard surge arresters often respond to TOVs with a 'safe failure', where the device is deactivated. ACI technology, on the other hand, offers high TOV withstand. That means an ACI device can withstand a temporary overvoltage and remain operational, rather than disconnecting from the mains. ACI devices feature galvanic isolation to prevent small fault currents from occurring, or they interrupt larger fault currents quickly and safely. 

How can TOV risks be managed?

ACI technology offers enhanced safety in the event of temporary power-frequency overvoltages up to at least 440 V. This high TOV withstand significantly reduces the risk of unexpected system failures caused by unstable mains conditions and enhances operational reliability. ACI closes this protection gap by reliably controlling even small fault currents that may occur during TOVs.  

Broken neutral conductor

A broken neutral conductor refers to an interruption or fault in the neutral conductor of an electrical system. This event is one of the primary causes of temporary power-frequency overvoltages, or TOVs. 

The consequences of a broken neutral conductor are serious and pose a particular challenge for surge protection:

TOVs and protection gaps

A broken neutral conductor leads to temporary power-frequency overvoltages (TOVs), which may persist for a prolonged period. TOVs can cause fault currents that are too low to rapidly trip an external fuse with a large rating, but are enough to destroy the varistors (MOVs) in conventional surge protective devices.

High energy dissipation and destruction:

Low prospective short-circuit currents, as can occur during TOVs, result in long fuse disconnection times. This results in a very high energy dissipation in the SPD, which can damage the device or even the entire distribution board. 

Fire hazard

Without a suitable overcurrent protective device that reacts quickly to this kind of fault current, there is a risk of fire. In the event of a fault, the high energy dissipation can damage the SPD or even the entire distribution board.

How a broken neutral conductor can lead to a protection gap

Temporary power-frequency overvoltages are among the most common consequences of broken neutral conductors. If these fault currents are not detected and limited, the surge protective device, the distribution board and the connected equipment may be damaged.  

Selectivity in surge protection

Selective surge protection is crucial for the operational safety and availability of electrical installations. It ensures that, in the event of a fault, only the protective device directly affected trips, preventing unnecessary shutdowns of the entire system. Selectivity between overcurrent protective devices is also a requirement of the DIN VDE 0100-430 standard (Section 434). 

Targeted protection
What selectivity means

In the context of surge protection and overcurrent protective devices, selectivity means that, in the event of a fault, only the fuse directly affected trips.  

Full availability
Why selectivity is essential

Selectivity prevents a local fault from causing a total failure of the entire system and ensures that the power supply is maintained in the unaffected areas. 

Reliable coordination
Selectivity in standard-compliant planning

Selectivity between protective devices is a key component of standard-compliant system planning. Only when protective devices are coordinated to work together can faults be effectively contained and unnecessary shutdowns avoided.   

Cable routing and cross-sections in surge protection

Even if the right surge arresters have been selected and installed, they will only be effective if they are correctly integrated into the electrical system. In particular, the routing and sizing of the connecting cables are crucial factors that have a significant influence on the actual protection level provided at the terminal equipment. 

01
Voltage protection level

Long connecting cables cause additional voltage drops, which increase the effective protection level (Up) at the terminal equipment and reduce the SPD's effectiveness. External protective devices in the SPD path reinforce this effect. Short connecting cables improve surge protection. Up should not exceed 80% of the rated impulse withstand voltage for Category II. 

Mindestquerschnitte für sicheren Betrieb
02
Minimum cross-sections for safe operation

Connecting cables to the SPD must be able to withstand short-circuit currents. Minimum cross-sections are specified in the standards: 6 mm² of copper for Type 1 SPDs and 2.5 mm² of copper for Type 2 SPDs.  

03
Integrated overcurrent protection

ACI devices feature integrated overcurrent protection, which eliminates the voltage drop across external backup fuses. This keeps the protection level consistently low.

Installation für wirksamen Schutz
04
Installation for effective protection

Correct cable routing and minimal cable lengths are crucial for surge protection. Only a precise, standard-compliant installation ensures the required protection level at the terminal equipment and provides optimum protection for the electronics. Poor routing reduces SPD effectiveness.  

What is ISCCR?

The short-circuit withstand capability (ISCCR)  indicates the maximum short-circuit current that an SPD can safely handle. The specified short-circuit withstand capability (ISCCR)  of an SPD must be at least equal to the maximum short-circuit current expected at the connection point. This is crucial for operational safety and the protection of the electrical system. 

 

Glossary

ACI  

Advanced Circuit Interruption (ACI) is a technology that incorporates overcurrent protection into the surge protection device (SPD) itself. This eliminates the need for an external backup fuse, prevents any protection gaps and keeps the protection level consistently low.  

SPD  

SPD stands for Surge Protective Device and is the internationally used term for this equipment, which protects electrical systems and equipment from transient overvoltages. 

Up  

The protection level (Up) describes the maximum voltage applied to the SPD during a discharge event. The lower the voltage protection level, the better the protection for connected devices. It must not exceed the rated impulse withstand voltage (Uw) of the equipment to be protected and is influenced by cable lengths and external backup fuses. 

Uc  

The maximum continuous operating voltage (Uc) is the maximum effective voltage that an SPD can withstand continuously during normal operation without tripping. Its value depends on the type of system (TN, TT or IT system) and the connection point. 

In  

The nominal discharge current (In) describes an SPD's ability to discharge surge currents multiple times without being damaged. For Type 2 SPDs, the nominal impulse discharge current at the system's feeding point must comply with specified values.  

Iimp  

The lightning impulse current (Iimp) describes an SPD's ability to safely discharge partial lightning currents. It is the key characteristic value of Type 1 SPDs. 

ISCCR  

The short-circuit withstand capability (ISCCR) is the maximum prospective short-circuit current of the electrical network for which the SPD, together with its disconnectors, is rated. It must be at least equal to the maximum short-circuit current expected at the connection point.  

TOV  

TOV stands for temporary overvoltages and refers to temporary power-frequency overvoltages that may persist for a prolonged period, for example as a result of a broken neutral conductor.  

Selectivity  

Selectivity means that, in the event of a fault, only the protective device or SPD directly affected trips, while upstream protective devices remain operational. This prevents unnecessary system failures and increases the availability of the entire electrical system.  

Lightning current  

A lightning current is a high-energy current impulse caused by a direct or indirect lightning strike. Type 1 SPDs are specifically designed to divert these significant currents, where Iimp is the relevant characteristic value. 

Fault current 

A fault current is an unintended flow of current caused by a fault in the electrical system, such as an ageing SPD or a TOV event. Small fault currents can create a protection gap, where external fuses do not respond quickly enough to prevent damage to the SPD. 

Broken neutral conductor 

A broken neutral conductor creates an interruption in the neutral conductor within an electrical system. It can cause temporary power-frequency overvoltages (TOVs) and result in significant damage to electrical equipment.  

Protection gap 

The protection gap refers to a critical fault current range between the SPD and the external backup fuse. In this range, the SPD can be damaged even before the fuse trips.  

Varistor (MOV) 

A varistor (metal oxide varistor) is the key protective component in many surge protective devices. It limits overvoltages by diverting excess energy, protecting connected devices.  

Type 1 SPD 

Type 1 SPDs provide protection against high partial lightning currents, which may occur, for example, in an external lightning protection system or an overhead line supply. They are usually installed at the system's feeding point. 

 

 

 

Type 2 SPD 

Type 2 SPDs protect against transient overvoltages caused by switching operations or indirect lightning. They are typically used in main and sub-distribution boards. 

 

Type 3 SPD 

Type 3 SPDs are used to provide secondary protection for sensitive terminal equipment. They are installed as close as possible to the equipment to be protected and complement Type 1 and Type 2 SPDs. 

In-depth topics

From protection gaps and ACI technology to standards and applications, the following topics will help you to better understand the technical intricacies and make informed decisions when it comes to planning and installing surge protection.

Downloads

Register now for DEHNinfo

We would be happy to keep you up to date with information on lightning and surge protection and safety equipment.

Exclusive industry news and trends
DEHN product innovations
Changes in standards

Any questions?

Write us a message.

I agree to the processing of my personal data in accordance with the Data Privacy Statement. Take me to the Data Privacy Statement.

 
Here you will find all information about the processing of your personal data.
CAPTCHA
This question tests whether you are human or a computer and prevents automated spam submissions.